ElbowSnapSettings Class¶
-
class
NXOpen.Routing.
ElbowSnapSettings
¶ Bases:
NXOpen.Builder
Helper object used the by
NXOpen.Routing.LinearPathBuilder
builder.Determines whether or not elbow snapping should occur in the “Create Linear Path” UI, and if so, what the angle tolerance should be.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateElbowSnapSettings()
Default values.
Property Value AngleTolerance 5.0 SnapToElbowAngles True New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the tolerance within which to search for elbow angles. |
SnapToElbowAngles | Returns or sets whether or not to snap control points to the nearest valid elbow angle. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
ElbowSnapSettings.
AngleTolerance
¶ Returns or sets the tolerance within which to search for elbow angles.
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AngleTolerance(tolerance)
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
SnapToElbowAngles¶
-
ElbowSnapSettings.
SnapToElbowAngles
¶ Returns or sets whether or not to snap control points to the nearest valid elbow angle.
-------------------------------------
Getter Method
Signature
SnapToElbowAngles()
Returns: Return type: bool New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
SnapToElbowAngles(doSnap)
Parameters: doSnap (bool) – New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
Validate¶
-
ElbowSnapSettings.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.