AnchorCollection Class¶
-
class
NXOpen.Routing.
AnchorCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.Anchor
objects.Iterating this collection only returns live uncondemned objects contained in the owning part of the collection. Note that
NXOpen.Routing.Anchor
is a smart object and many smart objects are condemned as they only exist to support other objects and are not displayed. Condemned objects will be deleted when their references go away. To obtain an instance of this class, refer toNXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateAnchor | Creates a NXOpen.Routing.Anchor object. |
Method Detail¶
CreateAnchor¶
-
AnchorCollection.
CreateAnchor
¶ Overloaded method CreateAnchor
CreateAnchor(origin)
CreateAnchor(position, point)
-------------------------------------
Creates a
NXOpen.Routing.Anchor
object.Signature
CreateAnchor(origin)
Parameters: origin ( NXOpen.Point3d
) – Origin of the AnchorReturns: Return type: NXOpen.Routing.Anchor
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates a
NXOpen.Routing.Anchor
object.Signature
CreateAnchor(position, point)
Parameters: - position (
NXOpen.Point3d
) – This can be None - point (
NXOpen.Point
) – Anchor to this. If this is GeometricUtilities.Point.NULL use position
Returns: Return type: New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------