ReuseLibraryReportInBom Enumeration¶
NXOpen.Routing.ReuseLibrary.ReportInBom is an alias for NXOpen.Routing.ReuseLibraryReportInBom
-
class
NXOpen.Routing.
ReuseLibraryReportInBom
¶ Bases:
object
Represents the report in BOM logical type.
Enum Members
Enum Member Enum Member Description DoNotReport Do not report in the Bill of MaterialsReport Report in the Bill of Materials-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-