DesignRuleViolation Class¶
-
class
NXOpen.Routing.
DesignRuleViolation
¶ Bases:
NXOpen.NXObject
Represents
NXOpen.Routing.DesignRuleViolation
objectDesign Rule Violation object is created automatically during design rule check
New in version NX4.0.2.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
LongDescription | Returns or sets the long description of the design rule violation is returned |
Name | Returns the custom name of the object. |
Override | Returns or sets the override object for the violation is inquired |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
ShortDescription | Returns or sets the short description of the design rule violation is returned |
Tag | Returns the Tag for this object. |
TimeStamp | Returns or sets the date/time stamp of the violation is inquired |
Methods¶
Method | Description |
---|---|
AddObjects | Add an object in violation to the violation |
AddViolationLocations | This will add given number of violation location objects. |
BlankLocationObjectsOfViolation | This function will blank location objects of given violation. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteRuleOverride | Override object will be deleted |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLocations | This will give all violation location objects stored in calling violation object. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetObjects | Get the array of objects in violation @return Caller frees the array |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetViolationLocation | This will return violation location object stored at given postion of array. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
IsRuleOverridden | Violation is overridden or not is inquired @return |
Prints a representation of this object to the system log file. | |
RemoveViolationOverride | Removes violation override from given violation object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetLocations | |
SetName | Sets the custom name of the object. |
SetObjects | Sets the array of objects in violation |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetViolationLocation | This will set violation location object at given postion of array. |
SetViolationOverride | Sets the violation override |
Enumerations¶
DesignRuleViolationBlankOption Enumeration | Design Rule Violation Location Object Blank Option |
Property Detail¶
IsOccurrence¶
-
DesignRuleViolation.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
DesignRuleViolation.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
LongDescription¶
-
DesignRuleViolation.
LongDescription
¶ Returns or sets the long description of the design rule violation is returned
-------------------------------------
Getter Method
Signature
LongDescription()
Returns: Violation Description Return type: str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
LongDescription(longDescription)
Parameters: longDescription (str) – New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Name¶
-
DesignRuleViolation.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Override¶
-
DesignRuleViolation.
Override
¶ Returns or sets the override object for the violation is inquired
-------------------------------------
Getter Method
Signature
Override()
Returns: Return type: NXOpen.Routing.DesignRuleOverride
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Override(overrideTag)
Parameters: overrideTag ( NXOpen.Routing.DesignRuleOverride
) –New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
OwningComponent¶
-
DesignRuleViolation.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
DesignRuleViolation.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
DesignRuleViolation.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ShortDescription¶
-
DesignRuleViolation.
ShortDescription
¶ Returns or sets the short description of the design rule violation is returned
-------------------------------------
Getter Method
Signature
ShortDescription()
Returns: Violation Description Return type: str New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ShortDescription(shortDescription)
Parameters: shortDescription (str) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
TimeStamp¶
-
DesignRuleViolation.
TimeStamp
¶ Returns or sets the date/time stamp of the violation is inquired
-------------------------------------
Getter Method
Signature
TimeStamp()
Returns: Return type: int New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
TimeStamp(timeStamp)
Parameters: timeStamp (int) – New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
AddObjects¶
-
DesignRuleViolation.
AddObjects
¶ Add an object in violation to the violation
Signature
AddObjects(objects)
Parameters: objects (list of NXOpen.Routing.DesignRuleViolation
) –New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
AddViolationLocations¶
-
DesignRuleViolation.
AddViolationLocations
¶ This will add given number of violation location objects.
Signature
AddViolationLocations(locationObjects)
Parameters: locationObjects (list of NXOpen.Routing.DesignRuleViolationLocation
) – Array of violation locations to be added.New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
BlankLocationObjectsOfViolation¶
-
DesignRuleViolation.
BlankLocationObjectsOfViolation
¶ This function will blank location objects of given violation.
Signature
BlankLocationObjectsOfViolation(blankOption)
Parameters: blankOption ( NXOpen.Routing.DesignRuleViolationBlankOption
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
DeleteRuleOverride¶
-
DesignRuleViolation.
DeleteRuleOverride
¶ Override object will be deleted
Signature
DeleteRuleOverride(deleteObject)
Parameters: deleteObject ( NXOpen.Routing.DesignRuleOverride
) –New in version NX4.0.3.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindObject¶
-
DesignRuleViolation.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetLocations¶
-
DesignRuleViolation.
GetLocations
¶ This will give all violation location objects stored in calling violation object.
Signature
GetLocations()
Returns: Array of NXOpen.Routing.DesignRuleViolationLocation
object.Return type: list of NXOpen.Routing.DesignRuleViolationLocation
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetObjects¶
-
DesignRuleViolation.
GetObjects
¶ Get the array of objects in violation
Signature
GetObjects()
Returns: Caller frees the array Return type: list of NXOpen.NXObject
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetViolationLocation¶
-
DesignRuleViolation.
GetViolationLocation
¶ This will return violation location object stored at given postion of array.
If there is no object at the given position, it will give appropriate message. and return None
Signature
GetViolationLocation()
Returns: a tuple Return type: A tuple consisting of (locationObject, arrayPosition). locationObject is a NXOpen.Routing.DesignRuleViolationLocation
. ViolationLocation object at given array position. arrayPosition is a int.New in version NX6.0.0.
Deprecated since version NX8.0.3: Use
NXOpen.Routing.DesignRuleViolation.GetLocations()
instead.License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
IsRuleOverridden¶
-
DesignRuleViolation.
IsRuleOverridden
¶ Violation is overridden or not is inquired
Signature
IsRuleOverridden()
Returns: Return type: bool New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Print¶
-
DesignRuleViolation.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveViolationOverride¶
-
DesignRuleViolation.
RemoveViolationOverride
¶ Removes violation override from given violation object.
Signature
RemoveViolationOverride()
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetLocations¶
-
DesignRuleViolation.
SetLocations
¶ Signature
SetLocations(violationLocations)
Parameters: violationLocations (list of NXOpen.Routing.DesignRuleViolationLocation
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetName¶
-
DesignRuleViolation.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetObjects¶
-
DesignRuleViolation.
SetObjects
¶ Sets the array of objects in violation
Signature
SetObjects(objects)
Parameters: objects (list of NXOpen.NXObject
) – Caller frees the arrayNew in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetViolationLocation¶
-
DesignRuleViolation.
SetViolationLocation
¶ This will set violation location object at given postion of array.
If there is already an object at the given position, it will delete that object and set with new one.
Signature
SetViolationLocation(arrayPosition, locationObject)
Parameters: - arrayPosition (int) –
- locationObject (
NXOpen.Routing.DesignRuleViolationLocation
) – ViolationLocation object to be set at given array position.
New in version NX6.0.0.
Deprecated since version NX8.0.3: Use
NXOpen.Routing.DesignRuleViolation.AddViolationLocations()
instead.License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetViolationOverride¶
-
DesignRuleViolation.
SetViolationOverride
¶ Sets the violation override
Signature
SetViolationOverride(user, reason, timestamp)
Parameters: - user (str) –
- reason (str) –
- timestamp (int) –
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)