Method Enumeration¶
-
class
NXOpen.Routing.
Method
¶ Bases:
object
Available application methods for Overstock Applications for a given Overstock Enum Members
Enum Member Enum Member Description EntireSegments Cover all given segmentsInterval Cover the given segments intermittentlyPointToPoint Cover the given segments from one point to anotherPointAndLength Cover the given segments a point for a length-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-