SBendCorner Class¶
-
class
NXOpen.Routing.
SBendCorner
¶ Bases:
NXOpen.NXObject
The Routing SBendCorner defines a S-Bend.
There are 5 possible S-bend types.
The UI input is two work part line segment-ending RCPs, each of which implicitly provides a 3D point and vector. An S-bend heals the separation between the two segments with a C1 continuous spline segment.
To disambiguate among 5 S-bend types (see below), the user may need to further indicate whether the S-bend starts bending immediately at the end of one or both of the 2 input segments. Some arrangements of 2 segments do not require further user input to disambiguate among the possible S-bend types.
The direction vectors of the 2 input segments must either be perpendicular (types 1,2,3) or parallel (types 4,5).
The closest distance between the (infinite) lines containing the input segments must be less that twice the bend radius. If this condition does not hold, then 2 right angle bends could connect the 2 input segments, i.e., an S-bend is unnecessary.
Every S-bend has two bends, whose radii are always equal. Except for type 2 and 3, the bend angles are equal and in the range [ Pi/4, Pi/2 ].
S-bends never cause a cutback of an input segment, although type 1,2,4 S-bends may add a straight line extension to one of the segment ends before the bending starts. Type 1 S-bends may add a straight line extension to both segment ends.
INPUT
- R bend radius, which the user supplies, e.g., from a bend table.
- P1 Work part X,Y,Z of segment 1’s end.
- Vec1 Tangent at P1, pointing toward the open end of the segment.
- P2, Vec2 Similar to segment 1 above...
For computation solving purposes, the above input becomes a bend radius, height, width, and possibly a depth.
OUTPUT bend angle(s):
- a (alpha) (all S-bend types)
- g (gamma) (Type 3 only)
- Extension lengths, if any.
Bend angles are computed at the centers of the bend arcs
S-bends fall into two categories:
- End tangents are perpendicular.
Three types are possible. In the 3D diagrams below:
The constructor line, AB, is the perpendicular distance between the lines that the segments define.
- Height (H): length of A-B
- Depth (D): length of A-P1
- Width (W): length of B-P2
The A-B, A-P1, B-P2 vectors are mutually perpendicular.
- Features.SewBuilder.Type 1: does not have a middle straight line portion.
<code>
/ / seg1 P1 / * / / /
/ / / : A / : | : | , | , <ja_lt>—- bends meet (no straight segment) | : | : | -, | `-,_ +——————`-*———— B P2 seg2 </code>
The bend from segment 2 lies in the plane A,B,P2. The bend from segment 1 is always 90 degrees, and thus terminates somewhere in the plane A,B,P2. The bend from segment 1 always starts on an extension of segment 1 that is a distance R from A.
Segment 2 may also have to extend toward B before its bend starts.
Geometrically, the height is the sum of the vertical components of bend 1 and bend 2.
Type 2: middle straight line portion <code> / / seg1 P1 / * / / /
/ / / : A / : | : | | <ja_lt>—- straight segment | | <ja_lt>—– bend ends | -, | `-,_ +——————`-*———— B P2 seg2 </code>
Similar to Type 1:
The bend from segment 2 lies in the plane A,B,P2.
The bend from segment 1 is always 90 degrees, and thus terminates somewhere in the plane A,B,P2.
The bend from segment 1 always starts on an extension of segment 1 that is a distance R from A.
Unlike Type 1:
Segment 2’s bend always starts at P2, i.e., segment 2 never has an extension.
Type 3: middle straight line portion. user chooses between Type 2-3. <code> / / seg1 P1 / *
/ ‘ / ‘ / : <ja_lt>—- segment 1’s bend ends / | / | A / | | | <ja_lt>— straight segment | | | | | | | | | <ja_lt>—- segment 2’s bend ends | -,_ +—————--*———— B P2 seg2 </code>
The bend radius isn’t big enough to span the height so a middle straight line segment is necessary.
Neither segment can have an extension, i.e., the bends start at P1 and P2. Unlike in Type 2, segment 2’s bend does not lie in the plane A,B,P2, i.e., both bends immediately start bending toward each other.
End tangents are parallel, i.e., bend lies entirely within a plane. This category falls into two types.
Type 4: no middle straight line portion <code> seg1 P1 ————-. `. : <ja_lt>— where bends meet `, `-———*——– A E2 P2 seg2 </code>
The height, H, is length (A-P1), where A is the projection of P1 onto the line that seg2 defines.
Because both bend angles are the same, the bends meet at half the height H/2.
Type 5: middle straight line portion <code> seg1 P1 ————-. `. <ja_lt>— middle straight line segment `. `-———— A P2 seg2 </code>
The height, H, is length (A-P1), where A is the projection of P1 onto the line that seg2 defines. The width, W, is the A-P2 length.
Support Information:
o An extension as described above is the distance leading up to the bend arc.
Use the
NXOpen.Routing.SBendCornerCollection
to obtain an instance.New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSBendData | Returns the data for the S-Bend object @return TRUE: if bend ratio is used; FALSE: otherwise. |
GetSBendRadius | Gets the S-Bend radius of a S-Bend corner. |
GetSBendStocks | Returns an array of stocks for the S-Bend object @return Stock objects of the S-Bend corner. |
GetSegment | Gets the segment being used to represent the S-Bend. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSBendData | Set the data for the S-Bend object |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
SBendCorner.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SBendCorner.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SBendCorner.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SBendCorner.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SBendCorner.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SBendCorner.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
SBendCorner.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetSBendData¶
-
SBendCorner.
GetSBendData
¶ Returns the data for the S-Bend object
Signature
GetSBendData()
Returns: a tuple Return type: A tuple consisting of (useBendRatio, sbendType, startRcp, endRcp, segment, radiusOrRatio). useBendRatio is a bool. TRUE: if bend ratio is used; FALSE: otherwise. sbendType is a int. S-Bend type startRcp is a NXOpen.Routing.ControlPoint
. S-Bend start Control point endRcp is aNXOpen.Routing.ControlPoint
. S-Bend end Control point segment is aNXOpen.Routing.SplineSegment
. S-Bend segmentradiusOrRatio is a float. Bend radius or bend_ratio.New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetSBendRadius¶
-
SBendCorner.
GetSBendRadius
¶ Gets the S-Bend radius of a S-Bend corner.
Signature
GetSBendRadius()
Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetSBendStocks¶
-
SBendCorner.
GetSBendStocks
¶ Returns an array of stocks for the S-Bend object
Signature
GetSBendStocks()
Returns: Stock objects of the S-Bend corner. Return type: list of NXOpen.Routing.Stock
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetSegment¶
-
SBendCorner.
GetSegment
¶ Gets the segment being used to represent the S-Bend.
Signature
GetSegment()
Returns: Return type: NXOpen.Routing.SplineSegment
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Print¶
-
SBendCorner.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
SBendCorner.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetSBendData¶
-
SBendCorner.
SetSBendData
¶ Set the data for the S-Bend object
Signature
SetSBendData(sbendType, startRcp, endRcp, segment, radiusOrRatio, useBendRatio)
Parameters: - sbendType (int) – S-Bend type
- startRcp (
NXOpen.Routing.ControlPoint
) – The start Control point for the S-Bend. - endRcp (
NXOpen.Routing.ControlPoint
) – The end Control point for the S-Bend. - segment (
NXOpen.Routing.SplineSegment
) – S-Bend segment - radiusOrRatio (float) – S-Bend radius or bend_ratio.
- useBendRatio (bool) – TRUE: if bend ratio is used; FALSE: otherwise.
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)