IsoDrawingBuilder Class¶
-
class
NXOpen.Routing.
IsoDrawingBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Routing.IsoDrawingBuilder
, used to run the ISOGEN engine to create isometric drawings of piping networks.To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateIsoDrawingBuilder()
Default values.
Property Value DrawingTypesEnum System RunsToDrawTypesEnum All New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
DrawingTypesEnum | Returns or sets the selected drawing style |
OpenAfterCreation | Returns or sets the isometric drawing should be opened in NX after creation |
OutputFile | Returns or sets the name of the file which will contain the isometric drawing |
RunsSelection | Returns the routing runs selected to be included in the isometric drawing. |
RunsToDrawTypesEnum | Returns or sets the selected Runs to Draw type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
IsoDrawingBuilderDrawingTypes Enumeration | The drawing style selection enumeration. |
IsoDrawingBuilderRunsToDrawTypes Enumeration | The Runs to Draw selection enumeration. |
Property Detail¶
DrawingTypesEnum¶
-
IsoDrawingBuilder.
DrawingTypesEnum
¶ Returns or sets the selected drawing style
-------------------------------------
Getter Method
Signature
DrawingTypesEnum()
Returns: Return type: NXOpen.Routing.IsoDrawingBuilderDrawingTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawingTypesEnum(drawingTypesEnum)
Parameters: drawingTypesEnum ( NXOpen.Routing.IsoDrawingBuilderDrawingTypes
) –New in version NX8.5.0.
License requirements: None.
OpenAfterCreation¶
-
IsoDrawingBuilder.
OpenAfterCreation
¶ Returns or sets the isometric drawing should be opened in NX after creation
-------------------------------------
Getter Method
Signature
OpenAfterCreation()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OpenAfterCreation(openAfterCreation)
Parameters: openAfterCreation (bool) – New in version NX8.5.0.
License requirements: None.
OutputFile¶
-
IsoDrawingBuilder.
OutputFile
¶ Returns or sets the name of the file which will contain the isometric drawing
-------------------------------------
Getter Method
Signature
OutputFile()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFile(filename)
Parameters: filename (str) – New in version NX8.5.0.
License requirements: None.
RunsSelection¶
-
IsoDrawingBuilder.
RunsSelection
¶ Returns the routing runs selected to be included in the isometric drawing.
-------------------------------------
Getter Method
Signature
RunsSelection()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.5.0.
License requirements: None.
RunsToDrawTypesEnum¶
-
IsoDrawingBuilder.
RunsToDrawTypesEnum
¶ Returns or sets the selected Runs to Draw type
-------------------------------------
Getter Method
Signature
RunsToDrawTypesEnum()
Returns: Return type: NXOpen.Routing.IsoDrawingBuilderRunsToDrawTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RunsToDrawTypesEnum(runsToDrawTypesEnum)
Parameters: runsToDrawTypesEnum ( NXOpen.Routing.IsoDrawingBuilderRunsToDrawTypes
) –New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
IsoDrawingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.