UnifyPathBuilder Class¶
-
class
NXOpen.Routing.
UnifyPathBuilder
¶ Bases:
NXOpen.Builder
Builder to unify
Routing.Stock
andAssemblies.Component
based on specified characteristic values.The builder takes a set of objects and replaces them with new objects that matches the given characterstics. To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateUnifyPathBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ReferenceObject | Returns the reference object used to extract characteristics to unify. |
RouteObjectCollector | Returns the routing object collector to select objects to unify. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUnifyCharacteristics | Returns Routing.CharacteristicList to be used to find matching Routing.Stock and Assemblies.Component to replace. |
SetUnifyCharacteristics | Sets the characteristics to be applied |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ReferenceObject¶
-
UnifyPathBuilder.
ReferenceObject
¶ Returns the reference object used to extract characteristics to unify.
-------------------------------------
Getter Method
Signature
ReferenceObject()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RouteObjectCollector¶
-
UnifyPathBuilder.
RouteObjectCollector
¶ Returns the routing object collector to select objects to unify.
-------------------------------------
Getter Method
Signature
RouteObjectCollector()
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
GetUnifyCharacteristics¶
-
UnifyPathBuilder.
GetUnifyCharacteristics
¶ Returns
Routing.CharacteristicList
to be used to find matchingRouting.Stock
andAssemblies.Component
to replace.Signature
GetUnifyCharacteristics()
Returns: The characteristics to use in finding a replacement for the given object. Return type: NXOpen.Routing.CharacteristicList
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetUnifyCharacteristics¶
-
UnifyPathBuilder.
SetUnifyCharacteristics
¶ Sets the characteristics to be applied
Signature
SetUnifyCharacteristics(charxType, charxName, charxValue)
Parameters: - charxType (
NXOpen.NXObjectAttributeType
) – - charxName (str) –
- charxValue (str) – The characteristics to use in finding a replacement for the given object.
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- charxType (
Validate¶
-
UnifyPathBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.