DesignRuleViolationLocationCollectionDeleteOption Enumeration¶
NXOpen.Routing.DesignRuleViolationLocationCollection.DeleteOption is an alias for NXOpen.Routing.DesignRuleViolationLocationCollectionDeleteOption
-
class
NXOpen.Routing.
DesignRuleViolationLocationCollectionDeleteOption
¶ Bases:
object
Design Rule Violation Location object delete option
Enum Members
Enum Member Enum Member Description DoDelete DontDelete Set this option only if you do not want to delete violation location objects-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-