TerminalPort Class¶
-
class
NXOpen.Routing.
TerminalPort
¶ Bases:
NXOpen.Routing.Port
,NXOpen.Routing.IAxisPort
A
NXOpen.Routing.TerminalPort
models the pins on an electrical connector.NXOpen.Routing.TerminalPort`s are a :py:class:`NXOpen.Routing.MultiPort
‘s children.New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AllowMultipleConnections | Returns or sets the Allow Multiple Connections property for a NXOpen.Routing.Port . |
Axis | Returns or sets the axis that defines the port |
ClockIncrementObject | Returns or sets the clock angle increment expression of a NXOpen.Routing.Port , i. |
Color | Returns or sets the color of the object. |
CutbackLengthObject | Returns or sets the cutback length object of a port, i. |
EngagementObject | Returns or sets the engagement object of a port, i. |
ForwardExtensionObject | Returns or sets the forward extension object of a port, i. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
MultiPort | Returns the parent NXOpen.Routing.MultiPort of the NXOpen.Routing.TerminalPort |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PinIdentifier | Returns or sets the pin identifier (name) of the NXOpen.Routing.TerminalPort |
Point | Returns or sets the NXOpen.Point that specifies the location of the NXOpen.Routing.IRoutePosition object. |
Position | Returns or sets the current location of the object in ABS coordinates. |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Update | Returns the update option. |
Visibility | Returns the visibility. |
Methods¶
Method | Description |
---|---|
AskFeature | Ask NXOpen.Routing.FeaturePort object associated with NXOpen.Routing.Port . |
Blank | Blanks the object. |
Connect | Finds another NXOpen.Routing.Port to connect this port to. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCharacterstics | Removes the input list of characteristics from this object. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Disconnect | Deletes any NXOpen.Routing.PortConnection objects that reference this port. |
Evaluate | Evaluate a smart object. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FindPortIntegerCharacteristic | Searches for an integer characteristics on the port, then on the ports component and prototype port if the port is an occurrence. |
FindPortRealCharacteristic | Searches for a real characteristics on the port, then on the ports component and prototype port if the port is an occurrence. |
FindPortStringCharacteristic | Searches for a string characteristics on the port, then on the ports component and prototype port if the port is an occurrence. |
GetAlignmentVector | Retrieves the alignment vector of Port @return Vector direction in absolute co-ordinate system |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetClockIncrement | The clock angle increment value of NXOpen.Routing.Port @return Clock increment value in degrees |
GetComponent | If this port is an occurrence, returns the component part to which it belongs. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetConnectedPorts | If port is connected to another port, returns both connected ports. |
GetControlPoint | Returns the Routing.ControlPoint to which this port is constrained, if any. |
GetCutbackLength | Returns the cutback length of a port, i. |
GetDestinationCharacteristics | Returns the destination characteristics from the input object. |
GetEngagement | Returns the engagement distance of a port, i. |
GetFlowDirection | Get the value of flow direction of NXOpen.Routing.Port @return |
GetForwardExtension | Returns the forward extension value for a port i. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerCharacteristic | Get the value of an integer characteristic associated with the input name. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPortConnection | If port is connected to another port, returns the Port Connection that links them. |
GetPortType | Get the type of Port @return Port Type |
GetRealAttribute | Gets a real attribute by title. |
GetRealCharacteristic | Get the value of a real characteristic associated with the input name. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetReferenceCharacteristic | Gets a reference characteristic from the port. |
GetRotationObject | Retrieves the object used to derive the rotation vector of Port @return Object used to derive the rotation vector |
GetRotationVector | Retrieves the rotation vector of Port @return Vector direction in absolute co-ordinate system |
GetSegment | Return the segment the port position and alignment are derived from Returns None if the port is not derived from segment @return ISegment from which the port is derived |
GetStockOfPort | For a Routing.StockPort , returns the Routing.Stock to which this port is attached, if any. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringCharacteristic | Get the value of a string characteristic associated with the input name. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Highlight | Highlights the object. |
IsEngagementLocked | Checks to see if ports are engaged. |
IsRotationLocked | Checks if ports have their rotation vectors locked. |
LockEngagement | Locks the port engagement using dcm3 constraints @return Newly created port constraints |
LockRotation | Locks the port rotation vector using dcm3 constraints @return Newly created port constraints |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveParameters | Removes the smart object parameters. |
RemoveViewDependency | Remove dependency on all views from an object. |
ReorderFeature | Reorders the NXOpen.Routing.FeaturePort object associated with NXOpen.Routing.Port after all of the features on which the port feature depends. |
ReplaceParameters | Edit a smart object by replacing its parameters using parameters of other smart object of the same class. |
SetAlignVector | Sets the align vector of Port |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristic | Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. |
SetCharacteristic2 | Sets or creates an integer type attribute associated with the input title. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetCharacteristics2 | Sets all attributes associated with the titles from the input list, creating new attributes for the ones that don’t exist already. |
SetClockIncrement | The clock angle increment value of NXOpen.Routing.Port |
SetCutbackLength | Sets the cutback length of a port, i. |
SetEngagement | The engagment distance of a NXOpen.Routing.IAxisPort , i. |
SetFlowDirection | Set the flow direction value of NXOpen.Routing.Port |
SetForwardExtension | Sets the forward extension value of a port, i. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetReferenceCharacteristic | Sets a reference characteristics on the port. |
SetRotationObject | Sets the object used to derive the rotation vector of Port |
SetRotationVector | Sets the rotation vector of Port |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetVisibility | Sets the visibility. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
UnlockEngagement | Unlocks the port engagement |
UnlockRotation | Unlocks the port rotation |
Property Detail¶
Axis¶
-
TerminalPort.
Axis
¶ Returns or sets the axis that defines the port
-------------------------------------
Getter Method
Signature
Axis()
Returns: Return type: NXOpen.Axis
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Axis(axis)
Parameters: axis ( NXOpen.Axis
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
CutbackLengthObject¶
-
TerminalPort.
CutbackLengthObject
¶ Returns or sets the cutback length object of a port, i.
e. an expression representing the length along the wire from the port where individual wires leave a bundle to attach to pins
-------------------------------------
Getter Method
Signature
CutbackLengthObject()
Returns: Cutback Length Expression Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
CutbackLengthObject(cutbackLength)
Parameters: cutbackLength ( NXOpen.Expression
) – Cutback Length ExpressionNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
EngagementObject¶
-
TerminalPort.
EngagementObject
¶ Returns or sets the engagement object of a port, i.
e. an expression representing the distance behind the port that another fitting or stock may engage
-------------------------------------
Getter Method
Signature
EngagementObject()
Returns: Engagement Expression Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
EngagementObject(engagement)
Parameters: engagement ( NXOpen.Expression
) – Engagement ExpressionNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
ForwardExtensionObject¶
-
TerminalPort.
ForwardExtensionObject
¶ Returns or sets the forward extension object of a port, i.
e. an expression representing the minimum length that a segment must remain straight coming out of a
NXOpen.Routing.Port
-------------------------------------
Getter Method
Signature
ForwardExtensionObject()
Returns: Forward Extension Expression Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ForwardExtensionObject(forwardExtension)
Parameters: forwardExtension ( NXOpen.Expression
) – Forward Extension ExpressionNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
IsOccurrence¶
-
TerminalPort.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
TerminalPort.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MultiPort¶
-
TerminalPort.
MultiPort
¶ Returns the parent
NXOpen.Routing.MultiPort
of theNXOpen.Routing.TerminalPort
-------------------------------------
Getter Method
Signature
MultiPort()
Returns: parent NXOpen.Routing.MultiPort
Return type: NXOpen.Routing.MultiPort
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Name¶
-
TerminalPort.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
TerminalPort.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
TerminalPort.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PinIdentifier¶
-
TerminalPort.
PinIdentifier
¶ Returns or sets the pin identifier (name) of the
NXOpen.Routing.TerminalPort
-------------------------------------
Getter Method
Signature
PinIdentifier()
Returns: pin identifier Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
PinIdentifier(pinIdentifier)
Parameters: pinIdentifier (str) – pin identifier New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Point¶
-
TerminalPort.
Point
¶ Returns or sets the
NXOpen.Point
that specifies the location of theNXOpen.Routing.IRoutePosition
object.A NULL object indicates that this object is not associated to any point.
-------------------------------------
Getter Method
Signature
Point()
Returns: New location of object in ABS coordinates Return type: NXOpen.Point
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) – New location of object in ABS coordinatesNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Position¶
-
TerminalPort.
Position
¶ Returns or sets the current location of the object in ABS coordinates.
This value is overridden by the coordinates of the point associated with this object.
-------------------------------------
Getter Method
Signature
Position()
Returns: Location of object in ABS coordinates Return type: NXOpen.Point3d
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Position(position)
Parameters: position ( NXOpen.Point3d
) – New location of object in ABS coordinatesNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Prototype¶
-
TerminalPort.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
DeleteCharacterstics¶
-
TerminalPort.
DeleteCharacterstics
¶ Removes the input list of characteristics from this object.
Signature
DeleteCharacterstics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindObject¶
-
TerminalPort.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetCharacteristics¶
-
TerminalPort.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetDestinationCharacteristics¶
-
TerminalPort.
GetDestinationCharacteristics
¶ Returns the destination characteristics from the input object.
Retrieves the description of which destination characteristics to read from the application view and then reads those destination characteristics from the object
- Ports: Reads characteristics from the port.
- RCPs: Attempts to find a port at the RCP, reads characteristics from
the port if it exists, otherwise reads from the stock associated with the rcp.
- Segments: Reads characteristics from the stock associated with the segment.
- Components: Reads characteristics directly from the component.
- Stock: Reads characteristics from the stock or from the stock’s data.
Signature
GetDestinationCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetIntegerCharacteristic¶
-
TerminalPort.
GetIntegerCharacteristic
¶ Get the value of an integer characteristic associated with the input name.
Signature
GetIntegerCharacteristic(name)
Parameters: name (str) – Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetRealCharacteristic¶
-
TerminalPort.
GetRealCharacteristic
¶ Get the value of a real characteristic associated with the input name.
Signature
GetRealCharacteristic(name)
Parameters: name (str) – Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetStringCharacteristic¶
-
TerminalPort.
GetStringCharacteristic
¶ Get the value of a string characteristic associated with the input name.
Signature
GetStringCharacteristic(name)
Parameters: name (str) – Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Print¶
-
TerminalPort.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetAlignVector¶
-
TerminalPort.
SetAlignVector
¶ Sets the align vector of Port
Signature
SetAlignVector(vector)
Parameters: vector ( NXOpen.Vector3d
) – Vector direction in absolute co-ordinate systemNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetCharacteristic¶
-
TerminalPort.
SetCharacteristic
¶ Overloaded method SetCharacteristic
SetCharacteristic(name, value)
SetCharacteristic(name, value)
SetCharacteristic(name, value)
-------------------------------------
Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to integer if it’s type is not integer.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (int) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an real characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to real if it’s type is not real.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (float) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an string characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to string if it’s type is not string.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (str) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristic2¶
-
TerminalPort.
SetCharacteristic2
¶ Overloaded method SetCharacteristic2
SetCharacteristic2(title, value)
SetCharacteristic2(title, value)
SetCharacteristic2(title, value)
-------------------------------------
Sets or creates an integer type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (int) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets or creates a double type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (float) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets or creates a string type type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (str) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristics¶
-
TerminalPort.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristics2()
instead.License requirements: routing_base (“Routing Basic”)
SetCharacteristics2¶
-
TerminalPort.
SetCharacteristics2
¶ Sets all attributes associated with the titles from the input list, creating new attributes for the ones that don’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit part attributes on the stock part. For legacy parts where the attributes are on the stock component, the attributes will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit attributes on the corresponding instance. For legacy parts where the attribute is on the component, the attributes will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create attributes on the object itself.
Signature
SetCharacteristics2(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –NXOpen.Routing.CharacteristicList
having the titles, types and values of Attributes to be setNew in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
SetCutbackLength¶
-
TerminalPort.
SetCutbackLength
¶ Sets the cutback length of a port, i.
e. the length along the wire from the port where individual wires leave a bundle to attach to pins
Signature
SetCutbackLength(cutbackLength)
Parameters: cutbackLength (float) – Cutback Length New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetEngagement¶
-
TerminalPort.
SetEngagement
¶ The engagment distance of a
NXOpen.Routing.IAxisPort
, i.e. the distance behind the port that another fitting or stock may engage
Signature
SetEngagement(engagement)
Parameters: engagement (float) – Engagement distance New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetForwardExtension¶
-
TerminalPort.
SetForwardExtension
¶ Sets the forward extension value of a port, i.
e. the minimum length that a segment must remain straight coming out of a
NXOpen.Routing.Port
Signature
SetForwardExtension(forwardExtension)
Parameters: forwardExtension (float) – Port extension New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetName¶
-
TerminalPort.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetRotationObject¶
-
TerminalPort.
SetRotationObject
¶ Sets the object used to derive the rotation vector of Port
Signature
SetRotationObject(rotationObject)
Parameters: rotationObject ( NXOpen.DisplayableObject
) – Object used to derive the rotation vectorNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetRotationVector¶
-
TerminalPort.
SetRotationVector
¶ Sets the rotation vector of Port
Signature
SetRotationVector(vector)
Parameters: vector ( NXOpen.Vector3d
) – Vector direction in absolute co-ordinate systemNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)