ControlPointCollection Class¶
-
class
NXOpen.Routing.
ControlPointCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.ControlPoint
objects.Iterating this collection only returns live uncondemned objects contained in the owning part of the collection. Note that
NXOpen.Routing.ControlPoint
is a smart object and many smart objects are condemned as they only exist to support other objects and are not displayed. Condemned objects will be deleted when their references go away. To obtain an instance of this class, refer toNXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateControlPoint | Creates a dumb NXOpen.Routing.ControlPoint object. |
FindControlPoint | Finds an existing NXOpen.Routing.ControlPoint at the given ABS coordinates within the given tolerance. |
Enumerations¶
ControlPointCollectionCheckExisting Enumeration | Option for searching for an existing NXOpen.Routing.ControlPoint when attempting to create an new NXOpen.Routing.ControlPoint . |
ControlPointCollectionFoundExisting Enumeration | Whether NXOpen.Routing.ControlPoint returned from the creator methods was an existing NXOpen.Routing.ControlPoint or a new NXOpen.Routing.ControlPoint . |
Method Detail¶
CreateControlPoint¶
-
ControlPointCollection.
CreateControlPoint
¶ Overloaded method CreateControlPoint
CreateControlPoint(position, checkExisting)
CreateControlPoint(port, checkExisting)
CreateControlPoint(object, objectParm, checkExisting)
CreateControlPoint(point, checkExisting)
CreateControlPoint(conic, checkExisting)
CreateControlPoint(startObject, offset, checkExisting)
CreateControlPoint(cpOcc, checkExisting)
-------------------------------------
Creates a dumb
NXOpen.Routing.ControlPoint
object. TheNXOpen.Routing.ControlPoint
‘s position is not associative to any other object.Signature
CreateControlPoint(position, checkExisting)
Parameters: - position (
NXOpen.Point3d
) – ABS coordinates - checkExisting (
NXOpen.Routing.ControlPointCollectionCheckExisting
) – Return an existingNXOpen.Routing.ControlPoint
object if one exists at the same location as the position.
Returns: a tuple
Return type: A tuple consisting of (controlpoint, foundExisting). controlpoint is a
NXOpen.Routing.ControlPoint
. foundExisting is aNXOpen.Routing.ControlPointCollectionFoundExisting
. ReturnedNXOpen.Routing.ControlPoint
is an existing control point.New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates a smart
NXOpen.Routing.ControlPoint
object. TheNXOpen.Routing.ControlPoint
‘s position is associative to the inputNXOpen.Routing.Port
.Signature
CreateControlPoint(port, checkExisting)
Parameters: - port (
NXOpen.Routing.Port
) – - checkExisting (
NXOpen.Routing.ControlPointCollectionCheckExisting
) – Return an existingNXOpen.Routing.ControlPoint
object if one exists at the same location as the position.
Returns: a tuple
Return type: A tuple consisting of (controlpoint, foundExisting). controlpoint is a
NXOpen.Routing.ControlPoint
. foundExisting is aNXOpen.Routing.ControlPointCollectionFoundExisting
. ReturnedNXOpen.Routing.ControlPoint
is an existing control point.New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates a
NXOpen.Routing.ControlPoint
at the given object and normalized parameter. Supports curves [includes segments], ports and circular edges.Signature
CreateControlPoint(object, objectParm, checkExisting)
Parameters: - object (
NXOpen.TaggedObject
) – - objectParm (float) –
- checkExisting (
NXOpen.Routing.ControlPointCollectionCheckExisting
) – Return an existingNXOpen.Routing.ControlPoint
object if one exists at the same location as the position.
Returns: a tuple
Return type: A tuple consisting of (controlpoint, foundExisting). controlpoint is a
NXOpen.Routing.ControlPoint
. foundExisting is aNXOpen.Routing.ControlPointCollectionFoundExisting
. ReturnedNXOpen.Routing.ControlPoint
is an existing control point.New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates a smart
NXOpen.Routing.ControlPoint
object. TheNXOpen.Routing.ControlPoint
‘s position is associative to the inputNXOpen.Point
.Signature
CreateControlPoint(point, checkExisting)
Parameters: - point (
NXOpen.Point
) – - checkExisting (
NXOpen.Routing.ControlPointCollectionCheckExisting
) – Return an existingNXOpen.Routing.ControlPoint
object if one exists at the same location as the position.
Returns: a tuple
Return type: A tuple consisting of (controlpoint, foundExisting). controlpoint is a
NXOpen.Routing.ControlPoint
. foundExisting is aNXOpen.Routing.ControlPointCollectionFoundExisting
. ReturnedNXOpen.Routing.ControlPoint
is an existing control point.New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates a smart
NXOpen.Routing.ControlPoint
object. TheNXOpen.Routing.ControlPoint
‘s position is associative to aNXOpen.Point
that is defined at the center of aNXOpen.IBaseCurve
object.Signature
CreateControlPoint(conic, checkExisting)
Parameters: - conic (
NXOpen.IBaseCurve
) – - checkExisting (
NXOpen.Routing.ControlPointCollectionCheckExisting
) – Return an existingNXOpen.Routing.ControlPoint
object if one exists at the same location as the position.
Returns: a tuple
Return type: A tuple consisting of (controlpoint, foundExisting). controlpoint is a
NXOpen.Routing.ControlPoint
. foundExisting is aNXOpen.Routing.ControlPointCollectionFoundExisting
. ReturnedNXOpen.Routing.ControlPoint
is an existing control point.New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates a dumb
NXOpen.Routing.ControlPoint
object. TheNXOpen.Routing.ControlPoint
‘s position is not associative to any other object. The position of the object is located at the XC, YC, ZC offset (using the work coordinate system) from the inputNXOpen.Routing.IRoutePosition
object.Signature
CreateControlPoint(startObject, offset, checkExisting)
Parameters: - startObject (
NXOpen.Routing.IRoutePosition
) – Starting position. - offset (
NXOpen.Vector3d
) – Offset values. - checkExisting (
NXOpen.Routing.ControlPointCollectionCheckExisting
) – Return an existingNXOpen.Routing.ControlPoint
object if one exists at the same location as the position.
Returns: a tuple
Return type: A tuple consisting of (controlpoint, foundExisting). controlpoint is a
NXOpen.Routing.ControlPoint
. foundExisting is aNXOpen.Routing.ControlPointCollectionFoundExisting
. ReturnedNXOpen.Routing.ControlPoint
is an existing control point.New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates a smart
NXOpen.Routing.ControlPoint
object. TheNXOpen.Routing.ControlPoint
‘s position is smart point that is associative to aNXOpen.Point
that is associative to aNXOpen.Routing.ControlPoint
occurrence.Signature
CreateControlPoint(cpOcc, checkExisting)
Parameters: - cpOcc (
NXOpen.Routing.ControlPoint
) – Occurrence of aNXOpen.Routing.ControlPoint
object. - checkExisting (
NXOpen.Routing.ControlPointCollectionCheckExisting
) – Return an existingNXOpen.Routing.ControlPoint
object if one exists at the same location as the position.
Returns: a tuple
Return type: A tuple consisting of (controlpoint, foundExisting). controlpoint is a
NXOpen.Routing.ControlPoint
. foundExisting is aNXOpen.Routing.ControlPointCollectionFoundExisting
. ReturnedNXOpen.Routing.ControlPoint
is an existing control point.New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
FindControlPoint¶
-
ControlPointCollection.
FindControlPoint
¶ Finds an existing
NXOpen.Routing.ControlPoint
at the given ABS coordinates within the given tolerance.Signature
FindControlPoint(position, tolerance)
Parameters: - position (
NXOpen.Point3d
) – ABS coordinates - tolerance (float) – Distance tolerance, smallest useful tolerance is returned from
NXOpen.Routing.RouteManager.GetLengthTolerance()
.
Returns: Return type: New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- position (