ControlPointDefinedStatus Enumeration¶
NXOpen.Routing.ControlPoint.DefinedStatus is an alias for NXOpen.Routing.ControlPointDefinedStatus
-
class
NXOpen.Routing.
ControlPointDefinedStatus
¶ Bases:
object
User defined status for a
NXOpen.Routing.ControlPoint
.Enum Members
Enum Member Enum Member Description System Created automatically by the application.User Created by the user.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-