FittingOverstockBuilderTrimMethod Enumeration¶
NXOpen.Routing.FittingOverstockBuilder.TrimMethod is an alias for NXOpen.Routing.FittingOverstockBuilderTrimMethod
-
class
NXOpen.Routing.
FittingOverstockBuilderTrimMethod
¶ Bases:
object
Trimming option.
This defines the way the selected faces are to be trimmed for
NXOpen.Routing.FittingOverstockBuilderTypes.PartialFace
method.Enum Members
Enum Member Enum Member Description TrimPlane Single Trim PlaneBetweenPlanes Double Trim Planes-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-