FindByAttributesBuilder Class¶
-
class
NXOpen.Routing.
FindByAttributesBuilder
¶ Bases:
NXOpen.Builder
Find runs/objects with specified attribute name and attribute value criteria, highlight the corresponding nodes in the run navigator and the graphics area
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateFindByAttributesBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AttribList | Returns the attribute list containing search criteria |
AttributeName | Returns or sets the string containing attribute title to search for |
AttributeValue | Returns or sets the string containing attribute value to search for |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AttributeMembersBuilder | Creates an AttributeMembersBuilder object used to create list item @return |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
HighlightRunNavItems | Highlight/Unhighlight the search results for FindByAttributes |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AttribList¶
-
FindByAttributesBuilder.
AttribList
¶ Returns the attribute list containing search criteria
-------------------------------------
Getter Method
Signature
AttribList()
Returns: Return type: NXOpen.TaggedObjectList
New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
AttributeName¶
-
FindByAttributesBuilder.
AttributeName
¶ Returns or sets the string containing attribute title to search for
-------------------------------------
Getter Method
Signature
AttributeName()
Returns: Return type: str New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AttributeName(attributeName)
Parameters: attributeName (str) – New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
AttributeValue¶
-
FindByAttributesBuilder.
AttributeValue
¶ Returns or sets the string containing attribute value to search for
-------------------------------------
Getter Method
Signature
AttributeValue()
Returns: Return type: str New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AttributeValue(attributeValue)
Parameters: attributeValue (str) – New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
AttributeMembersBuilder¶
-
FindByAttributesBuilder.
AttributeMembersBuilder
¶ Creates an AttributeMembersBuilder object used to create list item
Signature
AttributeMembersBuilder()
Returns: Return type: NXOpen.Routing.AttributeMembersBuilder
New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Validate¶
-
FindByAttributesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.