SplinePathBuilderSplinePathSlackType Enumeration¶
NXOpen.Routing.SplinePathBuilder.SplinePathSlackType is an alias for NXOpen.Routing.SplinePathBuilderSplinePathSlackType
-
class
NXOpen.Routing.
SplinePathBuilderSplinePathSlackType
¶ Bases:
object
Describes the method the spline is defined as.
Enum Members
Enum Member Enum Member Description PercentLength A control point (Thru-Point) spline.AdditionalLength A interpolating (By-Poles) spline.Undefined The spline is undefined.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-