OverstockBuilder Class¶
-
class
NXOpen.Routing.
OverstockBuilder
¶ Bases:
NXOpen.Builder
Builder for creating/editing overstocks.
Create Overstock: This builder takes a set of segments and overstock and assign the the overstock on the segments depending on the applicatio method and parameters chosen by the user. Edit Overstock: This builder takes in the selected overstock to edit as input and redefines the overstock with the modified(by the user) parameters.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateOverstockBuilder()
Default values.
Property Value ApplicationMethod Interval Distance.Value 0 (millimeters part), 0 (inches part) DistanceLock 0 EndOffsetLock 0 FlipStock 0 Gap.Value 0 (millimeters part), 0 (inches part) GapDistance.Value 1 (millimeters part), 1 (inches part) GapLock 0 IntervalPieceLength.Value 0 (millimeters part), 0 (inches part) NumberOfPieces.Value 1 (millimeters part), 1 (inches part) NumberOfPiecesLock 0 NumberOfWraps.Value 2 (millimeters part), 2 (inches part) OverlapPercentage.Value 50 (millimeters part), 50 (inches part) PieceLength.Value 0 (millimeters part), 0 (inches part) PieceLengthLock 0 PointDefines Start RotationValue.Value 0 StartOffsetLock 0 SwapProfile 0 WrapMethod OverlapSpiral New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ApplicationMethod | Returns or sets the application method for overstock assignment. |
DefiningPoint | Returns the defining point for :py:class:` NXOpen.Routing.OverstockBuilderApplicationType.PointAndLength < NXOpen.Routing.OverstockBuilderApplicationType>` method. |
Distance | Returns the distance over which the pieces of overstock can possibly range for NXOpen.Routing.OverstockBuilderApplicationType.Interval method. |
DistanceLock | Returns or sets the distance lock state. |
EndOffset | Returns the end offset value for NXOpen.Routing.OverstockBuilderApplicationType.Interval method. |
EndOffsetLock | Returns or sets the end offset lock state. |
EndPoint | Returns the end point that defines the end of the overstock for NXOpen.Routing.OverstockBuilderApplicationType.PointToPoint method. |
FlipStock | Returns or sets the stock flip flag |
Gap | Returns the gap from the end of one piece of overstock to the start of the next piece of overstock for NXOpen.Routing.OverstockBuilderApplicationType.Interval method. |
GapDistance | Returns the gap distance if the NXOpen.Routing.OverstockBuilderWrapType is NXOpen.Routing.OverstockBuilderWrapType.StripedSpiral |
GapLock | Returns or sets the gap lock state. |
IntervalPieceLength | Returns the length of the overstock pieces for NXOpen.Routing.OverstockBuilderApplicationType.Interval method. |
NumberOfPieces | Returns the number of pieces of overstock to place along the path for NXOpen.Routing.OverstockBuilderApplicationType.Interval method. |
NumberOfPiecesLock | Returns or sets the number of pieces lock state. |
NumberOfWraps | Returns the number of wraps if the NXOpen.Routing.OverstockBuilderWrapType is NXOpen.Routing.OverstockBuilderWrapType.Spot |
OverlapPercentage | Returns the percentage overlap if the NXOpen.Routing.OverstockBuilderWrapType is NXOpen.Routing.OverstockBuilderWrapType.OverlapSpiral |
PathCurve | Returns the path curve that is used to specify overstock defining points. |
PieceLength | Returns the length over which overstock piece to be assigned for NXOpen.Routing.OverstockBuilderApplicationType.PointAndLength method. |
PieceLengthLock | Returns or sets the piece length lock state. |
PointDefines | Returns or sets the defining point location which can be any of NXOpen.Routing.OverstockBuilderPointType for :py:class:` NXOpen.Routing.OverstockBuilderApplicationType.PointAndLength < NXOpen.Routing.OverstockBuilderApplicationType>` method. |
RotationValue | Returns the rotation value. |
SegmentCollector | Returns the routing object collector to collect the segments to assign overstock to. |
StartOffset | Returns the start offset value for NXOpen.Routing.OverstockBuilderApplicationType.Interval method. |
StartOffsetLock | Returns or sets the start offset lock state. |
StartPoint | Returns the start point that defines the start of the overstock for NXOpen.Routing.OverstockBuilderApplicationType.PointToPoint method. |
StockAnchor | Returns or sets the NXOpen.Routing.Anchor name associated with the overstock. |
StockSettings | Returns or sets the stock settings for overstock assignment. |
SwapProfile | Returns or sets the profile swap flag. |
SwitchStartEnd | Returns or sets the path direction that defines the start of overstock assignment. |
Tag | Returns the Tag for this object. |
WrapMethod | Returns or sets the NXOpen.Routing.OverstockBuilderWrapType for Wrapped overstock. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCoveredStocks | Returns the stocks to be covered by the overstock. |
GetObject | Returns the object currently being edited by this builder. |
SetCoveredStocks | Sets the stocks to be covered by the overstock. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdatePathCurve | Update the path curve that is used to specify overstock defining points when any segment is selected or deselected. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
OverstockBuilderApplicationType Enumeration | The overstock application type. |
OverstockBuilderPointType Enumeration | The defining point location. |
OverstockBuilderWrapType Enumeration | The application type for wrapped overstock |
Property Detail¶
ApplicationMethod¶
-
OverstockBuilder.
ApplicationMethod
¶ Returns or sets the application method for overstock assignment.
It defines the way in which to create piggyback segment for overstock.
-------------------------------------
Getter Method
Signature
ApplicationMethod()
Returns: Return type: NXOpen.Routing.OverstockBuilderApplicationType
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
ApplicationMethod(applicationMethod)
Parameters: applicationMethod ( NXOpen.Routing.OverstockBuilderApplicationType
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
DefiningPoint¶
-
OverstockBuilder.
DefiningPoint
¶ Returns the defining point for :py:class:` NXOpen.Routing.OverstockBuilderApplicationType.PointAndLength < NXOpen.Routing.OverstockBuilderApplicationType>` method.
-------------------------------------
Getter Method
Signature
DefiningPoint()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
Distance¶
-
OverstockBuilder.
Distance
¶ Returns the distance over which the pieces of overstock can possibly range for
NXOpen.Routing.OverstockBuilderApplicationType.Interval
method.-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
DistanceLock¶
-
OverstockBuilder.
DistanceLock
¶ Returns or sets the distance lock state.
If TRUE, changing the parameters will change other unlocked parameters to fit overstock along the selected path.
-------------------------------------
Getter Method
Signature
DistanceLock()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
DistanceLock(distanceLock)
Parameters: distanceLock (bool) – New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
EndOffset¶
-
OverstockBuilder.
EndOffset
¶ Returns the end offset value for
NXOpen.Routing.OverstockBuilderApplicationType.Interval
method.It defins the MINIMUM distance from the end of the path to place the last piece of overstock.
-------------------------------------
Getter Method
Signature
EndOffset()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
EndOffsetLock¶
-
OverstockBuilder.
EndOffsetLock
¶ Returns or sets the end offset lock state.
If TRUE, changing the parameters will change other unlocked parameters to fit overstock along the selected path.
-------------------------------------
Getter Method
Signature
EndOffsetLock()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
EndOffsetLock(endOffsetLock)
Parameters: endOffsetLock (bool) – New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
EndPoint¶
-
OverstockBuilder.
EndPoint
¶ Returns the end point that defines the end of the overstock for
NXOpen.Routing.OverstockBuilderApplicationType.PointToPoint
method.-------------------------------------
Getter Method
Signature
EndPoint()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
FlipStock¶
-
OverstockBuilder.
FlipStock
¶ Returns or sets the stock flip flag
-------------------------------------
Getter Method
Signature
FlipStock()
Returns: Return type: bool New in version NX6.0.1.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
FlipStock(flipStock)
Parameters: flipStock (bool) – New in version NX6.0.1.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
Gap¶
-
OverstockBuilder.
Gap
¶ Returns the gap from the end of one piece of overstock to the start of the next piece of overstock for
NXOpen.Routing.OverstockBuilderApplicationType.Interval
method.-------------------------------------
Getter Method
Signature
Gap()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GapDistance¶
-
OverstockBuilder.
GapDistance
¶ Returns the gap distance if the
NXOpen.Routing.OverstockBuilderWrapType
isNXOpen.Routing.OverstockBuilderWrapType.StripedSpiral
-------------------------------------
Getter Method
Signature
GapDistance()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GapLock¶
-
OverstockBuilder.
GapLock
¶ Returns or sets the gap lock state.
If TRUE, changing the parameters will change other unlocked parameters to fit overstock along the selected path.
-------------------------------------
Getter Method
Signature
GapLock()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
GapLock(gapLock)
Parameters: gapLock (bool) – New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
IntervalPieceLength¶
-
OverstockBuilder.
IntervalPieceLength
¶ Returns the length of the overstock pieces for
NXOpen.Routing.OverstockBuilderApplicationType.Interval
method.If the overstock type is Wrapped, and the wrap method is set to Spot, the Piece Length is always the width of the overstock and is locked.
-------------------------------------
Getter Method
Signature
IntervalPieceLength()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
NumberOfPieces¶
-
OverstockBuilder.
NumberOfPieces
¶ Returns the number of pieces of overstock to place along the path for
NXOpen.Routing.OverstockBuilderApplicationType.Interval
method.-------------------------------------
Getter Method
Signature
NumberOfPieces()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
NumberOfPiecesLock¶
-
OverstockBuilder.
NumberOfPiecesLock
¶ Returns or sets the number of pieces lock state.
If TRUE, changing the parameters will change other unlocked parameters to fit overstock along the selected path.
-------------------------------------
Getter Method
Signature
NumberOfPiecesLock()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
NumberOfPiecesLock(numberOfPiecesLock)
Parameters: numberOfPiecesLock (bool) – New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
NumberOfWraps¶
-
OverstockBuilder.
NumberOfWraps
¶ Returns the number of wraps if the
NXOpen.Routing.OverstockBuilderWrapType
isNXOpen.Routing.OverstockBuilderWrapType.Spot
-------------------------------------
Getter Method
Signature
NumberOfWraps()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
OverlapPercentage¶
-
OverstockBuilder.
OverlapPercentage
¶ Returns the percentage overlap if the
NXOpen.Routing.OverstockBuilderWrapType
isNXOpen.Routing.OverstockBuilderWrapType.OverlapSpiral
-------------------------------------
Getter Method
Signature
OverlapPercentage()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
PathCurve¶
-
OverstockBuilder.
PathCurve
¶ Returns the path curve that is used to specify overstock defining points.
-------------------------------------
Getter Method
Signature
PathCurve()
Returns: Return type: NXOpen.Curve
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
PieceLength¶
-
OverstockBuilder.
PieceLength
¶ Returns the length over which overstock piece to be assigned for
NXOpen.Routing.OverstockBuilderApplicationType.PointAndLength
method.-------------------------------------
Getter Method
Signature
PieceLength()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
PieceLengthLock¶
-
OverstockBuilder.
PieceLengthLock
¶ Returns or sets the piece length lock state.
If TRUE, changing the parameters will change other unlocked parameters to fit overstock along the selected path.
-------------------------------------
Getter Method
Signature
PieceLengthLock()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
PieceLengthLock(pieceLengthLock)
Parameters: pieceLengthLock (bool) – New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
PointDefines¶
-
OverstockBuilder.
PointDefines
¶ Returns or sets the defining point location which can be any of
NXOpen.Routing.OverstockBuilderPointType
for :py:class:` NXOpen.Routing.OverstockBuilderApplicationType.PointAndLength < NXOpen.Routing.OverstockBuilderApplicationType>` method.-------------------------------------
Getter Method
Signature
PointDefines()
Returns: Return type: NXOpen.Routing.OverstockBuilderPointType
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
PointDefines(pointDefines)
Parameters: pointDefines ( NXOpen.Routing.OverstockBuilderPointType
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
RotationValue¶
-
OverstockBuilder.
RotationValue
¶ Returns the rotation value.
Determines the rotation angle of the overstock.
-------------------------------------
Getter Method
Signature
RotationValue()
Returns: Return type: NXOpen.Expression
New in version NX6.0.1.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
SegmentCollector¶
-
OverstockBuilder.
SegmentCollector
¶ Returns the routing object collector to collect the segments to assign overstock to.
-------------------------------------
Getter Method
Signature
SegmentCollector()
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
StartOffset¶
-
OverstockBuilder.
StartOffset
¶ Returns the start offset value for
NXOpen.Routing.OverstockBuilderApplicationType.Interval
method.It defines the distance from the beginning of the path to place the first piece of overstock.
-------------------------------------
Getter Method
Signature
StartOffset()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
StartOffsetLock¶
-
OverstockBuilder.
StartOffsetLock
¶ Returns or sets the start offset lock state.
If TRUE, changing the parameters will change other unlocked parameters to fit overstock along the selected path
-------------------------------------
Getter Method
Signature
StartOffsetLock()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
StartOffsetLock(startOffsetLock)
Parameters: startOffsetLock (bool) – New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
StartPoint¶
-
OverstockBuilder.
StartPoint
¶ Returns the start point that defines the start of the overstock for
NXOpen.Routing.OverstockBuilderApplicationType.PointToPoint
method.-------------------------------------
Getter Method
Signature
StartPoint()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
StockAnchor¶
-
OverstockBuilder.
StockAnchor
¶ Returns or sets the
NXOpen.Routing.Anchor
name associated with the overstock.-------------------------------------
Getter Method
Signature
StockAnchor()
Returns: Return type: str New in version NX6.0.1.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
StockAnchor(anchorName)
Parameters: anchorName (str) – New in version NX6.0.1.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
StockSettings¶
-
OverstockBuilder.
StockSettings
¶ Returns or sets the stock settings for overstock assignment.
-------------------------------------
Getter Method
Signature
StockSettings()
Returns: Return type: NXOpen.Routing.PathStockBuilder
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
StockSettings(stockBuilder)
Parameters: stockBuilder ( NXOpen.Routing.PathStockBuilder
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
SwapProfile¶
-
OverstockBuilder.
SwapProfile
¶ Returns or sets the profile swap flag.
Determines whether the profile should be at the path start or end.
-------------------------------------
Getter Method
Signature
SwapProfile()
Returns: Return type: bool New in version NX6.0.1.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
SwapProfile(swapProfile)
Parameters: swapProfile (bool) – New in version NX6.0.1.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
SwitchStartEnd¶
-
OverstockBuilder.
SwitchStartEnd
¶ Returns or sets the path direction that defines the start of overstock assignment.
-------------------------------------
Getter Method
Signature
SwitchStartEnd()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
SwitchStartEnd(switchStartEnd)
Parameters: switchStartEnd (bool) – New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
WrapMethod¶
-
OverstockBuilder.
WrapMethod
¶ Returns or sets the
NXOpen.Routing.OverstockBuilderWrapType
for Wrapped overstock.-------------------------------------
Getter Method
Signature
WrapMethod()
Returns: Return type: NXOpen.Routing.OverstockBuilderWrapType
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
WrapMethod(wrapMethod)
Parameters: wrapMethod ( NXOpen.Routing.OverstockBuilderWrapType
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
Method Detail¶
GetCoveredStocks¶
-
OverstockBuilder.
GetCoveredStocks
¶ Returns the stocks to be covered by the overstock.
Signature
GetCoveredStocks()
Returns: Return type: list of NXOpen.Routing.Stock
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
SetCoveredStocks¶
-
OverstockBuilder.
SetCoveredStocks
¶ Sets the stocks to be covered by the overstock.
Signature
SetCoveredStocks(stocks)
Parameters: stocks (list of NXOpen.Routing.Stock
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
UpdatePathCurve¶
-
OverstockBuilder.
UpdatePathCurve
¶ Update the path curve that is used to specify overstock defining points when any segment is selected or deselected.
Signature
UpdatePathCurve()
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
Validate¶
-
OverstockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.