WrapApplicationType Enumeration¶
-
class
NXOpen.Routing.
WrapApplicationType
¶ Bases:
object
Available application methods for wrapped overstock Enum Members
Enum Member Enum Member Description Unknown Unknown wrap applicationSpot Spot wrap application, i.e., 100% overlapOverlapped Overlapping spiral wrap application, e.g., [0-100)% overlapGapped Barber pole spiral wrap application, e.g., no overlap-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-