StockStyle Enumeration¶
-
class
NXOpen.Routing.
StockStyle
¶ Bases:
object
Available styles of
NXOpen.Routing.CrossSection
for a givenNXOpen.Routing.StockData
.A
NXOpen.Routing.StockData
may have at most oneNXOpen.Routing.CrossSection
of each type. Enum MembersEnum Member Enum Member Description NotSet No profile.Simple Simple profile.Detailed Detailed profile.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-