RouteLogicalAssociation Class¶
-
class
NXOpen.Routing.
RouteLogicalAssociation
¶ Bases:
NXOpen.NXObject
RouteLogicalAssociation object associates non-electrical components to electrical components.
Logical Associations have control objects and target objects. Meeting control object’s condition applies actions to target objects. Example: Control object is a
NXOpen.Routing.ISegment
and the target object is a clip or clamp which supports the harness. When the segment is routed (i.e. condition on control object is satisfied), the action is to suppress the target (clip or clamp) To obtain an instance of this class useNXOpen.Routing.RouteLogicalAssociationCollection
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddTarget | Adds target to Logical Assocition |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
EnableLogicalAssociation | Set Logical Association to enabled state or disabled state. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetControl | Retrieves the control for LogicalAssocition @return Control |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetRoutedCondition | Get the routed condition of a logical association object. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTargets | Get all the targets LogicalAssocition @return Targets of current logical association |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Perform | Performs the specified action (suppress or unsuppress) on the RouteLogicalAssociation Object |
Prints a representation of this object to the system log file. | |
Remove | Removes the RouteLogicalAssociation object |
RemoveTarget | Removes the target from Logical Assocition |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetControl | Sets the control for LogicalAssocition |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetRoutedCondition | Set the routed condition of a logical association object * The routed condition evaluates the state of the control object. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
RouteLogicalAssociation.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
RouteLogicalAssociation.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
RouteLogicalAssociation.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
RouteLogicalAssociation.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
RouteLogicalAssociation.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
RouteLogicalAssociation.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddTarget¶
-
RouteLogicalAssociation.
AddTarget
¶ Adds target to Logical Assocition
Signature
AddTarget(target)
Parameters: target ( NXOpen.NXObject
) – Target to addNew in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
EnableLogicalAssociation¶
-
RouteLogicalAssociation.
EnableLogicalAssociation
¶ Set Logical Association to enabled state or disabled state.
- True sets LAO to enabled state, False sets LAO to disabled state.
Signature
EnableLogicalAssociation(enable)
Parameters: enable (bool) – True or False New in version NX5.0.0.
License requirements: routing_harness (“Routing Harness”)
FindObject¶
-
RouteLogicalAssociation.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetControl¶
-
RouteLogicalAssociation.
GetControl
¶ Retrieves the control for LogicalAssocition
Signature
GetControl()
Returns: Control Return type: NXOpen.NXObject
New in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
GetRoutedCondition¶
-
RouteLogicalAssociation.
GetRoutedCondition
¶ Get the routed condition of a logical association object.
- The routed condition evaluates the state of the control object.
- True if condition is ROUTED, False if UNROUTED
Signature
GetRoutedCondition()
Returns: Return type: bool New in version NX5.0.0.
License requirements: routing_harness (“Routing Harness”)
GetTargets¶
-
RouteLogicalAssociation.
GetTargets
¶ Get all the targets LogicalAssocition
Signature
GetTargets()
Returns: Targets of current logical association Return type: list of NXOpen.NXObject
New in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
Perform¶
-
RouteLogicalAssociation.
Perform
¶ Performs the specified action (suppress or unsuppress) on the RouteLogicalAssociation Object
Signature
Perform()
New in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
Print¶
-
RouteLogicalAssociation.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
Remove¶
-
RouteLogicalAssociation.
Remove
¶ Removes the RouteLogicalAssociation object
Signature
Remove()
New in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
RemoveTarget¶
-
RouteLogicalAssociation.
RemoveTarget
¶ Removes the target from Logical Assocition
Signature
RemoveTarget(target)
Parameters: target ( NXOpen.NXObject
) – Target to removeNew in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
SetControl¶
-
RouteLogicalAssociation.
SetControl
¶ Sets the control for LogicalAssocition
Signature
SetControl(control)
Parameters: control ( NXOpen.NXObject
) – ControlNew in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
SetName¶
-
RouteLogicalAssociation.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetRoutedCondition¶
-
RouteLogicalAssociation.
SetRoutedCondition
¶ Set the routed condition of a logical association object * The routed condition evaluates the state of the control object.
- True if condition is ROUTED, False if UNROUTED
Signature
SetRoutedCondition(condition)
Parameters: condition (bool) – New in version NX5.0.0.
License requirements: routing_harness (“Routing Harness”)