Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Class and Description |
---|
AeroSheetmetalManager
Provides methods for manipulating the Knowledge Fusion rules in a part
To obtain an instance of this class, refer to FeatureCollection Created in NX4.0.0 |
SheetmetalManager
Represents an object that manages sheetmetal features
To obtain an instance of this class, refer to FeatureCollection Created in NX4.0.0 |
Class and Description |
---|
AdvancedFlangeBuilder
Represents a Sheetmetal Advanced Flange builder class.
|
AdvancedFlangeBuilder.Insets
This enum defines the material types
|
AdvancedFlangeBuilder.LengthReferences
This enum defines the flange length dimension types
|
AdvancedFlangeBuilder.Types
This enum defines the type options.
|
AeroFlangeBuilder
Represents a Aerospace Sheet Metal Flange Builder.
|
AeroFlangeBuilder.CompType
This method defines the types of Flange Compensation
|
AeroFlangeBuilder.DimType
This enum defines the flange length dimension types
|
AeroFlangeBuilder.DirType
This enum defines the type of direction vector
|
AeroFlangeBuilder.EndCompensationData
This class holds the data returned from
AeroFlangeBuilder.getEndCompensation(nxopen.features.sheetmetal.AeroFlangeBuilder.EndType) |
AeroFlangeBuilder.EndType
This enum defines the ends of a bend edge
|
AeroFlangeBuilder.LengthData
This class holds the data returned from
AeroFlangeBuilder.getLength() |
AeroFlangeBuilder.LengthType
This enum defines the length type options.
|
AeroFlangeBuilder.MatType
This enum defines the material types
|
AeroJoggleBuilder
Represents a Aerospace Sheet Metal Joggle Builder.
|
AeroJoggleBuilder.SideType
This enum defines the side of a twin joggle
only side1 is used for a single joggle
|
AeroLighteningCutoutBuilder
Represents a
AeroLighteningCutoutBuilder
To create a new instance of this class, use AeroSheetmetalManager.createAeroLighteningCutoutBuilder(nxopen.features.Feature) Default values. |
AeroLighteningCutoutBuilder.Types
Represents the cutout type.
|
AeroReformBuilder
Represents a Aerospace Sheet Metal REFORM Builder.
|
AeroUnformBuilder
Represents a Aerospace Sheet Metal UNFORM Builder.
|
ApplicationContext
This is the enum representing application context of the feature
|
BeadBuilder
Represents a Bead feature builder.
|
BeadBuilder.CrossSectionTypeOptions
This enum represents the cross section type options for the Bead.
|
BeadBuilder.EndTypeOptions
This enum represents the end type options for the Bead.
|
BeadBuilder.HeightSideOptions
This enum represents the depth direction for the Bead.
|
BendBuilder
Represents a Bend feature builder.
|
BendBuilder.BendDirectionOptions
This enum represents the Bend Direction for Bend.
|
BendBuilder.BendLocationOptions
This enum represents the Bend Location (Material Side) for Bend.
|
BendBuilder.FixedSideOptions
This enum represents the Fixed Side for Bend.
|
BendListBuilder
Represents a Sheetmetal Flat Pattern bend list builder class.
|
BendListItemBuilder
Represents a Sheetmetal Flat Pattern bend list item builder class.
|
BendListItemBuilderList
Represents a list of objects.
|
BendOptions
Represents a Sheetmetal Bend Options class.
|
BendOptions.BendReliefTypeOptions
This enum represents the bend relief type.
|
BendOptions.CornerReliefTypeOptions
This enum represents the corner relief type.
|
BendTaperBuilder
Represents a Bend Taper feature builder
To create a new instance of this class, use SheetmetalManager.createBendTaperBuilder(nxopen.features.Feature) Default values. |
BendTaperBuilder.BendTaperInputMethod
This enum represents the input methods for the bend taper.
|
BendTaperBuilder.BendTaperSides
This enum represents the taper sides options for the bend taper.
|
BendTaperBuilder.BendTaperType
This enum represents the bend taper types for the bend taper.
|
BendTaperBuilder.ChainingType
Deprecated.
Deprecated in NX8.5.0. Use WebTaperType instead.
|
BendTaperBuilder.StartType
This enum represents the start types for the bend taper.
|
BendTaperBuilder.WebTaperType
This enum represents the web taper types for the bend taper.
|
BreakCornerBuilder
Represents a break corner feature builder.
|
BreakCornerBuilder.TypeOptions
This enum represents the break corner type.
|
BridgeTransitionBuilder
Represents a Bridge Transition builder
To create a new instance of this class, use SheetmetalManager.createBridgeTransitionBuilder(nxopen.features.Feature) Created in NX5.0.2 |
BridgeTransitionBuilder.FoldTransitionTypeOptions
Enum representing the type of
BridgeTransitionBuilder.TypeOptions.FOLD . |
BridgeTransitionBuilder.InsetOptions
Enum representing the side of the Bridge Transition material with respect to
the specified tangent plane.
|
BridgeTransitionBuilder.TypeOptions
Enum representing types for Bridge Transition feature.
|
BridgeTransitionBuilder.WidthDirectionOptions
Enum representing the width direction for the Bridge Transition.
|
BridgeTransitionBuilder.WidthOptions
Enum representing width option types for Bridge Transition feature.
|
CleanUpUtilityBuilder
Represents a Clean-Up Utility builder builder
To create a new instance of this class, use SheetmetalManager.createCleanUpUtilityBuilder() Default values. |
ClosedCornerBuilder
Represents a Closed corner feature builder.
|
ClosedCornerBuilder.ClosureTypeOptions
This enum represents Corner Closure type
|
ClosedCornerBuilder.FacePairData
This class holds the data returned from
ClosedCornerBuilder.getFacePair(int) |
ClosedCornerBuilder.OriginTypes
This enum represents Origin type
|
ClosedCornerBuilder.TreatmentTypeOptions
This enum represents Corner treatment type
|
ClosedCornerBuilder.Types
This enum represents the feature types.
|
ContourFlangeBuilder
Represents a Contour Flange feature builder.
|
ContourFlangeBuilder.SectionSideOptions
This enum represents the side of the section in which material is created.
|
ContourFlangeBuilder.SweepSideOptions
This enum represents the side in which the contour flange will be swept.
|
ContourFlangeBuilder.SweepTypeOptions
This enum represents the sweep type of the contour flange
|
ConvertInputListItemBuilder
Represents a Sheetmetal convert to sheet metal corner list item builder class.
|
ConvertInputListItemBuilderList
Represents a list of objects.
|
ConvertToSheetmetalBuilder
This is the feature builder for the convert to sheetmetal feature.
|
ConvertToSheetmetalBuilder.BendReliefTypeOptions
This enum represents the bend relief type.
|
CornerTreatmentBuilder
The CornerTreatmentBuilder class is used to manage a builder object for
a corner treatment in the flat solid and flat pattern dialogs.
|
CornerTreatmentBuilder.CornerTreatmentType
Corner Treatment Type
|
DimpleBuilder
Represents a Dimple feature builder.
|
DimpleBuilder.DepthTypeOptions
This enum represents the depth direction for the dimple.
|
DimpleBuilder.DimensionTypeOptions
the Dimension options for dimple.
|
DimpleBuilder.SectionSideOptions
This enum represents the side of the section that the dimple punches material.
|
DimpleBuilder.SidewallTypeOptions
the side walls material option.
|
DrawnCutoutBuilder
Represents a Drawn Cutout feature builder.
|
DrawnCutoutBuilder.DepthTypeOptions
This enum represents the depth direction for the drawn cutout.
|
DrawnCutoutBuilder.SectionSideOptions
This enum represents the side of the section that the drawn cutout punches material.
|
DrawnCutoutBuilder.SidewallTypeOptions
The side walls material option.
|
EdgeRipBuilder
Represents a Edge Rip feature builder.
|
EditBendBuilder
Represents a
EditBend builder
To create a new instance of this class, use SheetmetalManager.createEditBendBuilder(nxopen.features.Feature) Created in NX7.5.0 |
EditCornerBuilder
Represents a
EditCornerBuilder
To create a new instance of this class, use SheetmetalManager.createEditCornerBuilder() Default values. |
EditCornerBuilder.BendClosureTypeOptions
This enum specifies the type of bend closure required at the corner.
|
EditCornerBuilder.CornerReliefTypeOptions
This enum specifies the type of relief required at the corner.
|
EditCornerBuilder.FacePairData
This class holds the data returned from
EditCornerBuilder.getFacePair(int) |
EditCornerBuilder.PlateClosureTypeOptions
This enum specifies the type of plate closure required at the corner.
|
ExportFlatPatternBuilder
Represents a Export flat pattern builder.
|
ExportFlatPatternBuilder.DxfRevisionType
Specifies the DXF Revisions for flat pattern export
|
ExportFlatPatternBuilder.FileType
Specifies the flat pattern export type
|
FeatureBendPropertiesBuilder
Represents a Sheetmetal Feature bend properties builder class.
|
FeatureBendPropertiesBuilderList
Represents a list of objects.
|
FeatureBendPropertiesListBuilder
Represents a Sheetmetal Feature properties List builder class.
|
FeatureProperty
This is a common enum that comprises of values to be used for various features.
|
FlangeBendPropertiesBuilder
Represents a Sheetmetal Flange Bend Properties builder class.
|
FlangeBendPropertiesBuilder.Insets
This enum defines the material inset types
|
FlangeBendPropertiesBuilder.LengthReferences
This enum defines the flange length dimension types
|
FlangeBendPropertiesBuilder.WidthOptions
This enum defines the flange width options
|
FlangeBuilder
Represents a Flange feature builder.
|
FlangeBuilder.InsetTypeOptions
This enum represents the inset type for the material of the flange.
|
FlangeBuilder.LengthTypeOptions
This enum indicates the two ways that the flange length can be measured.
|
FlangeBuilder.MatchFaceOptions
This enum represents the match face option for the flange.
|
FlangeBuilder.OffsetTypeOptions
This enum represents the offset type for the flange.
|
FlangeBuilder.WidthTypeOptions
This enum represents the width type for the flange.
|
FlatPatternBuilder
Represents a Flat Pattern feature builder.
|
FlatSolidBuilder
Represents a Flat As Solid feature builder.
|
FlatSolidBuilder.OrientationType
The enum defines how to orient flat solid body.
|
FlatSolidBuilder.TransformComponentsOption
The enum defines how to represent PCB components on flat solid.
|
FlexibleCableBuilder
Represents a Flexible Cable feature builder.
|
FlexibleCableBuilder.BendAngleDirectionOptions
This enum represents the bend angle direction for the bend segment.
|
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions
This enum represents the path adjustment angle direction for the bend segment.
|
FlexibleCableBuilder.SegmentTypeOptions
Represents the Flexible Cable segment options.
|
FlexibleCableSegment
Represents a Flexible Cable Segment class.
|
GussetBuilder
Represents a NX Sheet Metal
Gusset builder
To create a new instance of this class, use SheetmetalManager.createGussetBuilder(nxopen.features.Feature) Default values. |
GussetBuilder.PlacementOriginAndDirectionData
This class holds the data returned from
GussetBuilder.getPlacementOriginAndDirection() |
GussetBuilder.PlacementTypes
This enum represents the different options for placing an automatic profile Gusset.
|
GussetBuilder.Shapes
This enum represents the two different shapes for Gusset.
|
GussetBuilder.Types
This enum represents the two Gusset Feature types.
|
GussetBuilder.WidthSides
This enum represents the different options for thickening the user defined profile Gusset.
|
HemFlangeBuilder
Represents a
HemFlange builder
To create a new instance of this class, use SheetmetalManager.createHemFlangeFeatureBuilder(nxopen.features.Feature) Created in NX5.0.0 |
HemFlangeBuilder.BendReliefOptions
This enum represents the Bend relief type of the hem flange.
|
HemFlangeBuilder.InsetTypeOptions
This enum represents the inset type for the material of the hem flange.
|
HemFlangeBuilder.TypeOptions
Represents the Hem Flange type.
|
HoleTreatmentBuilder
The HoleTreatmentBuilder class is used to manage a builder object for
a hole treatment in the flat pattern dialogs.
|
HoleTreatmentBuilder.TreatmentType
Hole Treatment Type
|
JogBuilder
Represents a Jog feature builder.
|
JogBuilder.BendLocationOptions
Represents the bend location type.
|
JogBuilder.DimensionTypeOptions
the Dimension options for jog.
|
JogBuilder.DirectionTypeOptions
this enum represents the direction for the Jog.
|
JogBuilder.FixedSideOptions
The "left" option represents the side to the left of a person who is walking along the section in the direction of its curves
when the section normal is pointing up.
|
JoggleBuilder
Represents a Sheetmetal joggle builder class.
|
JoggleBuilder.LimitTypes
This enum defines the limit types
|
JoggleInputListItemBuilder
Represents a Sheetmetal joggle input list item builder class.
|
JoggleInputListItemBuilderList
Represents a list of objects.
|
JoggleSideOptionsBuilder
Represents a Sheetmetal Joggle side Options class.
|
LighteningCutout
Represents a lightening cutout feature
To create or edit an instance of this class, use LighteningCutoutBuilder Created in NX11.0.0 |
LighteningCutoutBuilder
Represents a
LighteningCutout builder To create a new instance of this class, use SheetmetalManager.createLighteningCutoutBuilder(nxopen.features.sheetmetal.LighteningCutout) Default values. |
LighteningCutoutBuilder.CutoutType
Represents the type of Lightening Cutout
|
LoftedFlangeBuilder
Represents a Lofted Flange feature builder.
|
LoftedFlangeBuilder.SectionSideOptions
This enum represents the side of the section that the lofted flange creates thickness.
|
LouverBuilder
Represents a louver feature builder.
|
LouverBuilder.DepthSideOptions
This enum represents the depth side for the louver.
|
LouverBuilder.EndTypeOptions
This enum represents the end type for the louver.
|
LouverBuilder.SectionSideOptions
This enum represents the side of the section that the louver width is measured.
|
MetaformBuilder
Represents a
Metaform builder
To create a new instance of this class, use SheetmetalManager.createMetaformBuilder(nxopen.features.Feature) Default values. |
MigratedPanelBuilder
Represents an I-DEAS Migrated Panel feature builder
This builder cannot be instantiated separately. |
MiterOptions
Represents a Miter Data Options builder.
|
MiterOptions.ClosedCornerTypeOptions
the closed corner type options.
|
MiterOptions.CornerTreatmentOriginTypeOptions
This enum represents corner treatment cutout origin type
|
MiterOptions.PositionOptions
the miter positions options.
|
MiterOptions.TypeOptions
the miter type options.
|
MultiBendBendPropertiesBuilder
Represents a Sheetmetal Multi Bend properties builder class.
|
MultiBendBendPropertiesBuilder.Insets
This enum defines the material inset types
|
MultiFlange
Represents a multi flange feature
To create or edit an instance of this class, use MultiFlangeBuilder Created in NX12.0.0 |
MultiFlangeBuilder
Represents a
MultiFlange builder
To create a new instance of this class, use SheetmetalManager.createMultiFlangeBuilder(nxopen.features.sheetmetal.MultiFlange) Created in NX12.0.0 |
MultiFlangeBuilder.MatchFaceOptions
This enum defines the mathc face options
|
NormalCutoutBuilder
Represents a NormalCutout feature builder.
|
NormalCutoutBuilder.CutTypeOptions
This enum represents the cut type for the normal cutout.
|
NormalCutoutBuilder.DepthSideOptions
This enum represents the depth direction for the normal cutout.
|
NormalCutoutBuilder.DepthTypeOptions
This enum represents the depth type for the normal cutout.
|
NormalCutoutBuilder.SectionSideOptions
This enum represents the side of the section that the normal cutout removes material.
|
NormalCutoutBuilder.TypeOptions
Represents the type of the normal cutout - sketch type OR 3D-curve type
|
RebendBuilder
The Rebend feature class.
|
ResizeBendAngleBuilder
Represents a
ResizeBendAngle builder
To create a new instance of this class, use SheetmetalManager.createResizeBendAngleBuilder(nxopen.features.Feature) Created in NX5.0.0 |
ResizeBendRadiusBuilder
Represents a ResizeBendRadius feature builder.
|
ResizeBendRadiusBuilder.BendReliefTypeOptions
This enum represents the bend relief type.
|
ResizeBendRadiusBuilder.Types
This enum represents the feature types.
|
ResizeNeutralFactorBuilder
Represents a Resize Neutral Factor Builder
To create a new instance of this class, use SheetmetalManager.createResizeNeutralFactorBuilder(nxopen.features.Feature) Created in NX5.0.0 |
SheetmetalBaseBuilder
Represents a Sheet Metal Feature Builder to be used in the creation and modification of features.
|
SheetmetalBendParameters
This structure contains the bend parameters for a Sheet Metal bend area.
|
SheetmetalBendState
Bend State
|
SheetmetalComponentBuilder
Represents a sheet metal component builder to be used in the creation and modification of features componenets.
|
SheetmetalFaceLayer
Face Layer
|
SheetmetalFaceType
Face Type
|
SheetMetalFromSolidBuilder
Represents a
SheetMetalFromSolid builder
(Sheet Metal from Solid). |
SheetmetalManager.InnerBendFacesData
This class holds the data returned from
SheetmetalManager.getInnerBendFaces(nxopen.Body) |
SheetmetalManagerFlangeWidthOption
Flange width option
|
SheetmetalManagerTabSweepDir
This enum is for Tab sweep direction flag.
|
SheetmetalManagerTabType
This is the enum for Tab type i.e. base tab and secondary tab.
|
SMBoundaryConditionBuilder
Represents a Boundary condition object for Metaform.
|
SMBoundaryConditionBuilder.ConstraintTypes
Types of Boundary condition constraints
|
SMBoundaryConditionBuilderList
Represents a list of objects.
|
SolidPunchBuilder
Represents a
SolidPunchBuilder
To create a new instance of this class, use SheetmetalManager.createSolidPunchBuilder(nxopen.features.Feature) Created in NX5.0.0 |
SolidPunchBuilder.Types
Represents the punch type
|
TabBuilder
Represents a Tab feature builder.
|
TabBuilder.SectionSideOptions
This enum represents the side of the section that the dimple punches material.
|
TabBuilder.ThicknessSideOptions
This enum represents the extent direction for the Tab.
|
ThreeBendCornerBuilder
The Three Bend Corner feature class.
|
ThreeBendCornerBuilder.FacePairData
This class holds the data returned from
ThreeBendCornerBuilder.getFacePair(int) |
ThreeBendCornerBuilder.OriginTypes
This enum represents Origin type
|
ThreeBendCornerBuilder.TreatmentTypeOptions
This enum represents the corner treatment type.
|
UnbendBuilder
The Unbend feature class.
|
Class and Description |
---|
FeatureProperty
This is a common enum that comprises of values to be used for various features.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.