Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static EditCornerBuilder.BendClosureTypeOptions |
EditCornerBuilder.BendClosureTypeOptions.CLOSED |
static EditCornerBuilder.BendClosureTypeOptions |
EditCornerBuilder.BendClosureTypeOptions.OPEN |
Modifier and Type | Method and Description |
---|---|
EditCornerBuilder.BendClosureTypeOptions |
EditCornerBuilder.bendClosureType()
Returns the bend type
License requirements: None. |
static EditCornerBuilder.BendClosureTypeOptions |
EditCornerBuilder.BendClosureTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EditCornerBuilder.BendClosureTypeOptions |
EditCornerBuilder.BendClosureTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EditCornerBuilder.BendClosureTypeOptions[] |
EditCornerBuilder.BendClosureTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EditCornerBuilder.setBendClosureType(EditCornerBuilder.BendClosureTypeOptions bends)
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.