Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static AdvancedFlangeBuilder.Insets |
AdvancedFlangeBuilder.Insets.BEND_OUTSIDE |
static AdvancedFlangeBuilder.Insets |
AdvancedFlangeBuilder.Insets.MATERIAL_INSIDE |
static AdvancedFlangeBuilder.Insets |
AdvancedFlangeBuilder.Insets.MATERIAL_OUTSIDE |
Modifier and Type | Method and Description |
---|---|
AdvancedFlangeBuilder.Insets |
AdvancedFlangeBuilder.inset()
Returns the inset type
License requirements: None. |
static AdvancedFlangeBuilder.Insets |
AdvancedFlangeBuilder.Insets.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AdvancedFlangeBuilder.Insets |
AdvancedFlangeBuilder.Insets.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AdvancedFlangeBuilder.Insets[] |
AdvancedFlangeBuilder.Insets.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AdvancedFlangeBuilder.setInset(AdvancedFlangeBuilder.Insets inset)
License requirements: adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.