public static class AdvancedFlangeBuilder.Insets extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BEND_OUTSIDE |
static int |
_MATERIAL_INSIDE |
static int |
_MATERIAL_OUTSIDE |
static AdvancedFlangeBuilder.Insets |
BEND_OUTSIDE |
static AdvancedFlangeBuilder.Insets |
MATERIAL_INSIDE |
static AdvancedFlangeBuilder.Insets |
MATERIAL_OUTSIDE |
Modifier and Type | Method and Description |
---|---|
static AdvancedFlangeBuilder.Insets |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AdvancedFlangeBuilder.Insets |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AdvancedFlangeBuilder.Insets[] |
values()
Returns an array that contains the values for this enum.
|
public static final AdvancedFlangeBuilder.Insets MATERIAL_INSIDE
public static final AdvancedFlangeBuilder.Insets MATERIAL_OUTSIDE
public static final AdvancedFlangeBuilder.Insets BEND_OUTSIDE
public static final int _MATERIAL_INSIDE
public static final int _MATERIAL_OUTSIDE
public static final int _BEND_OUTSIDE
public static AdvancedFlangeBuilder.Insets valueOf(int value)
public static AdvancedFlangeBuilder.Insets valueOf(String name)
public static AdvancedFlangeBuilder.Insets[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.