Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Method and Description |
---|---|
JoggleInputListItemBuilder |
JoggleBuilder.createJoggleInputListItem()
Create a input list item.
|
JoggleInputListItemBuilder |
JoggleInputListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
JoggleInputListItemBuilder[] |
JoggleInputListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
JoggleInputListItemBuilderList.append(JoggleInputListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
JoggleInputListItemBuilderList.append(JoggleInputListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
JoggleInputListItemBuilderList.erase(JoggleInputListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
JoggleInputListItemBuilderList.erase(JoggleInputListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
JoggleInputListItemBuilderList.findIndex(JoggleInputListItemBuilder obj)
Finds the index where the input object appears.
|
void |
JoggleInputListItemBuilderList.insert(int location,
JoggleInputListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
JoggleInputListItemBuilderList.setContents(JoggleInputListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
JoggleInputListItemBuilderList.swap(JoggleInputListItemBuilder object1,
JoggleInputListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.