Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static FlexibleCableBuilder.BendAngleDirectionOptions |
FlexibleCableBuilder.BendAngleDirectionOptions.NORMAL_DIRECTION
Bend angle normal direction.
|
static FlexibleCableBuilder.BendAngleDirectionOptions |
FlexibleCableBuilder.BendAngleDirectionOptions.REVERSE_NORMAL_DIRECTION
Bend angle reverse normal direction.
|
Modifier and Type | Method and Description |
---|---|
FlexibleCableBuilder.BendAngleDirectionOptions |
FlexibleCableSegment.bendAngleDirection()
Returns the bend angle direction.
|
static FlexibleCableBuilder.BendAngleDirectionOptions |
FlexibleCableBuilder.BendAngleDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlexibleCableBuilder.BendAngleDirectionOptions |
FlexibleCableBuilder.BendAngleDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlexibleCableBuilder.BendAngleDirectionOptions[] |
FlexibleCableBuilder.BendAngleDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
FlexibleCableSegment |
FlexibleCableBuilder.createBendSegment(String bendAngle,
String bendRadius,
String pathAdjustmentAngle,
FlexibleCableBuilder.BendAngleDirectionOptions bendAngleDirection,
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions pathAdjustmentAngleDirection,
int segmentIndex)
Creates a new
FlexibleCableSegment bend segment. |
void |
FlexibleCableSegment.setBendAngleDirection(FlexibleCableBuilder.BendAngleDirectionOptions bendAngleDirectionOption)
Sets the bend angle direction.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.