Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static SMBoundaryConditionBuilder.ConstraintTypes |
SMBoundaryConditionBuilder.ConstraintTypes.CURVE_ALONG_CURVE |
static SMBoundaryConditionBuilder.ConstraintTypes |
SMBoundaryConditionBuilder.ConstraintTypes.CURVE_TO_CURVE |
static SMBoundaryConditionBuilder.ConstraintTypes |
SMBoundaryConditionBuilder.ConstraintTypes.POINT_ALONG_CURVE |
static SMBoundaryConditionBuilder.ConstraintTypes |
SMBoundaryConditionBuilder.ConstraintTypes.POINT_TO_POINT |
Modifier and Type | Method and Description |
---|---|
SMBoundaryConditionBuilder.ConstraintTypes |
SMBoundaryConditionBuilder.constraintType()
Returns the constraint type
License requirements: None. |
static SMBoundaryConditionBuilder.ConstraintTypes |
SMBoundaryConditionBuilder.ConstraintTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SMBoundaryConditionBuilder.ConstraintTypes |
SMBoundaryConditionBuilder.ConstraintTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SMBoundaryConditionBuilder.ConstraintTypes[] |
SMBoundaryConditionBuilder.ConstraintTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SMBoundaryConditionBuilder.setConstraintType(SMBoundaryConditionBuilder.ConstraintTypes constraintType)
License requirements: adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.