Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static LighteningCutoutBuilder.CutoutType |
LighteningCutoutBuilder.CutoutType.HOLE |
static LighteningCutoutBuilder.CutoutType |
LighteningCutoutBuilder.CutoutType.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
LighteningCutoutBuilder.CutoutType |
LighteningCutoutBuilder.type()
Returns the type
License requirements: None. |
static LighteningCutoutBuilder.CutoutType |
LighteningCutoutBuilder.CutoutType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LighteningCutoutBuilder.CutoutType |
LighteningCutoutBuilder.CutoutType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LighteningCutoutBuilder.CutoutType[] |
LighteningCutoutBuilder.CutoutType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LighteningCutoutBuilder.setType(LighteningCutoutBuilder.CutoutType type)
License requirements: adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.