Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BendTaperBuilder.WebTaperType |
BendTaperBuilder.WebTaperType.FACE
Face
|
static BendTaperBuilder.WebTaperType |
BendTaperBuilder.WebTaperType.FACE_CHAIN
Face Chain
|
static BendTaperBuilder.WebTaperType |
BendTaperBuilder.WebTaperType.NONE
None
|
Modifier and Type | Method and Description |
---|---|
static BendTaperBuilder.WebTaperType |
BendTaperBuilder.WebTaperType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendTaperBuilder.WebTaperType |
BendTaperBuilder.WebTaperType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendTaperBuilder.WebTaperType[] |
BendTaperBuilder.WebTaperType.values()
Returns an array that contains the values for this enum.
|
BendTaperBuilder.WebTaperType |
BendTaperBuilder.webTaperType1()
Returns the web taper type for side 1
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
BendTaperBuilder.WebTaperType |
BendTaperBuilder.webTaperType2()
Returns the web taper type for side 2
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Modifier and Type | Method and Description |
---|---|
void |
BendTaperBuilder.setWebTaperType1(BendTaperBuilder.WebTaperType webTaperType1)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
void |
BendTaperBuilder.setWebTaperType2(BendTaperBuilder.WebTaperType webTaperType2)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.