Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static GussetBuilder.Types |
GussetBuilder.Types.AUTOMATIC_PROFILE
Gusset(s) will be created between the planar faces adjacent to the selected bend face.
|
static GussetBuilder.Types |
GussetBuilder.Types.USER_DEFINED_PROFILE
Gusset will be created using a profile defined by the user.
|
Modifier and Type | Method and Description |
---|---|
GussetBuilder.Types |
GussetBuilder.type()
Returns the type of Gusset feature
License requirements: None. |
static GussetBuilder.Types |
GussetBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GussetBuilder.Types |
GussetBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GussetBuilder.Types[] |
GussetBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GussetBuilder.setType(GussetBuilder.Types type)
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.