Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static FlangeBuilder.OffsetTypeOptions |
FlangeBuilder.OffsetTypeOptions.INSIDE
The flange is offset to the inside of the face
|
static FlangeBuilder.OffsetTypeOptions |
FlangeBuilder.OffsetTypeOptions.OUTSIDE
The flange is offset to the outside of the face
|
Modifier and Type | Method and Description |
---|---|
FlangeBuilder.OffsetTypeOptions |
FlangeBuilder.offsetType()
Returns the offset type for the flange.
|
static FlangeBuilder.OffsetTypeOptions |
FlangeBuilder.OffsetTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBuilder.OffsetTypeOptions |
FlangeBuilder.OffsetTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBuilder.OffsetTypeOptions[] |
FlangeBuilder.OffsetTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlangeBuilder.setOffsetType(FlangeBuilder.OffsetTypeOptions offsetType)
Sets the offset type for the flange.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.