Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BendTaperBuilder.StartType |
BendTaperBuilder.StartType.TAPER_FROM_BEND
Taper from Bend
|
static BendTaperBuilder.StartType |
BendTaperBuilder.StartType.TAPER_FROM_WEB
Taper from Web
|
Modifier and Type | Method and Description |
---|---|
BendTaperBuilder.StartType |
BendTaperBuilder.startType1()
Returns the start type for side 1
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
BendTaperBuilder.StartType |
BendTaperBuilder.startType2()
Returns the start type for side 2
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static BendTaperBuilder.StartType |
BendTaperBuilder.StartType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendTaperBuilder.StartType |
BendTaperBuilder.StartType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendTaperBuilder.StartType[] |
BendTaperBuilder.StartType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BendTaperBuilder.setStartType1(BendTaperBuilder.StartType startType1)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
void |
BendTaperBuilder.setStartType2(BendTaperBuilder.StartType startType2)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.