Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Interface and Description |
---|---|
interface |
FlangeBendPropertiesBuilder
Represents a Sheetmetal Flange Bend Properties builder class.
|
interface |
MultiBendBendPropertiesBuilder
Represents a Sheetmetal Multi Bend properties builder class.
|
Modifier and Type | Method and Description |
---|---|
FeatureBendPropertiesBuilder |
FeatureBendPropertiesListBuilder.createFeatureProperties()
Create a feature properties.
|
FeatureBendPropertiesBuilder |
FeatureBendPropertiesBuilderList.findItem(int index)
Returns the object at the input index.
|
FeatureBendPropertiesBuilder[] |
FeatureBendPropertiesBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
FeatureBendPropertiesBuilderList.append(FeatureBendPropertiesBuilder object)
Appends an object to the list
License requirements: None. |
void |
FeatureBendPropertiesBuilderList.append(FeatureBendPropertiesBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
FeatureBendPropertiesBuilderList.erase(FeatureBendPropertiesBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
FeatureBendPropertiesBuilderList.erase(FeatureBendPropertiesBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
FeatureBendPropertiesBuilderList.findIndex(FeatureBendPropertiesBuilder obj)
Finds the index where the input object appears.
|
void |
FeatureBendPropertiesBuilderList.insert(int location,
FeatureBendPropertiesBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
FeatureBendPropertiesBuilderList.setContents(FeatureBendPropertiesBuilder[] objects)
Sets the contents of the entire list.
|
void |
FeatureBendPropertiesBuilderList.swap(FeatureBendPropertiesBuilder object1,
FeatureBendPropertiesBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.