Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static NormalCutoutBuilder.SectionSideOptions |
NormalCutoutBuilder.SectionSideOptions.LEFT
Side pointed to by the inverse of the tangent cross normal vector
|
static NormalCutoutBuilder.SectionSideOptions |
NormalCutoutBuilder.SectionSideOptions.RIGHT
Side pointed to by the tangent cross normal vector
|
Modifier and Type | Method and Description |
---|---|
NormalCutoutBuilder.SectionSideOptions |
NormalCutoutBuilder.sectionSide()
Returns the side of the section that the normal cutout removes material.
|
static NormalCutoutBuilder.SectionSideOptions |
NormalCutoutBuilder.SectionSideOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NormalCutoutBuilder.SectionSideOptions |
NormalCutoutBuilder.SectionSideOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NormalCutoutBuilder.SectionSideOptions[] |
NormalCutoutBuilder.SectionSideOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NormalCutoutBuilder.setSectionSide(NormalCutoutBuilder.SectionSideOptions sectionSide)
Sets the side of the section that the normal cutout removes material.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.