Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static HoleTreatmentBuilder.TreatmentType |
HoleTreatmentBuilder.TreatmentType.CENTERMARK |
static HoleTreatmentBuilder.TreatmentType |
HoleTreatmentBuilder.TreatmentType.NONE |
Modifier and Type | Method and Description |
---|---|
HoleTreatmentBuilder.TreatmentType |
HoleTreatmentBuilder.treatment()
Returns the treatment type option menu value
License requirements: None. |
static HoleTreatmentBuilder.TreatmentType |
HoleTreatmentBuilder.TreatmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleTreatmentBuilder.TreatmentType |
HoleTreatmentBuilder.TreatmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleTreatmentBuilder.TreatmentType[] |
HoleTreatmentBuilder.TreatmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleTreatmentBuilder.setTreatment(HoleTreatmentBuilder.TreatmentType treatmentType)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.