Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BendOptions.CornerReliefTypeOptions |
BendOptions.CornerReliefTypeOptions.BEND_AND_FACE
igBendAndFaceCornerRelief
|
static BendOptions.CornerReliefTypeOptions |
BendOptions.CornerReliefTypeOptions.BEND_AND_FACE_CHAIN
igChainedCornerRelief
|
static BendOptions.CornerReliefTypeOptions |
BendOptions.CornerReliefTypeOptions.BEND_ONLY
igBendOnlyCornerRelief
|
static BendOptions.CornerReliefTypeOptions |
BendOptions.CornerReliefTypeOptions.NONE |
Modifier and Type | Method and Description |
---|---|
BendOptions.CornerReliefTypeOptions |
BendOptions.cornerReliefType()
Returns the corner relief type.
|
static BendOptions.CornerReliefTypeOptions |
BendOptions.CornerReliefTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendOptions.CornerReliefTypeOptions |
BendOptions.CornerReliefTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendOptions.CornerReliefTypeOptions[] |
BendOptions.CornerReliefTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BendOptions.setCornerReliefType(BendOptions.CornerReliefTypeOptions type)
Sets the corner relief type.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.