Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static AeroFlangeBuilder.MatType |
AeroFlangeBuilder.MatType.BEND_OUTSIDE
Bend Outside
|
static AeroFlangeBuilder.MatType |
AeroFlangeBuilder.MatType.MATERIAL_INSIDE
Material Inside
|
static AeroFlangeBuilder.MatType |
AeroFlangeBuilder.MatType.MATERIAL_OUTSIDE
Material Outside
|
Modifier and Type | Method and Description |
---|---|
AeroFlangeBuilder.MatType |
AeroFlangeBuilder.getMaterialType()
Get the material type of the flange
License requirements: aero_sheet_metal ("Aerospace Sheet Metal") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
static AeroFlangeBuilder.MatType |
AeroFlangeBuilder.MatType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AeroFlangeBuilder.MatType |
AeroFlangeBuilder.MatType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AeroFlangeBuilder.MatType[] |
AeroFlangeBuilder.MatType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AeroFlangeBuilder.setMaterialType(AeroFlangeBuilder.MatType matType)
Set the material type of the flange
License requirements: aero_sheet_metal ("Aerospace Sheet Metal") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.