Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static MiterOptions.CornerTreatmentOriginTypeOptions |
MiterOptions.CornerTreatmentOriginTypeOptions.BEND_CENTER
The cutout origin will be at the intersection of first bend's centerline and bisector of corner angle.
|
static MiterOptions.CornerTreatmentOriginTypeOptions |
MiterOptions.CornerTreatmentOriginTypeOptions.CORNER_POINT
The cutout origin will be at the corner point.
|
Modifier and Type | Method and Description |
---|---|
MiterOptions.CornerTreatmentOriginTypeOptions |
MiterOptions.cornerTreatmentOriginType()
Returns the origin used for circular, u and v cutout corner treatments.
|
static MiterOptions.CornerTreatmentOriginTypeOptions |
MiterOptions.CornerTreatmentOriginTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MiterOptions.CornerTreatmentOriginTypeOptions |
MiterOptions.CornerTreatmentOriginTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MiterOptions.CornerTreatmentOriginTypeOptions[] |
MiterOptions.CornerTreatmentOriginTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MiterOptions.setCornerTreatmentOriginType(MiterOptions.CornerTreatmentOriginTypeOptions originType)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.