Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static MiterOptions.ClosedCornerTypeOptions |
MiterOptions.ClosedCornerTypeOptions.CIRCULAR_CUTOUT
corner has a circular cutout in it
|
static MiterOptions.ClosedCornerTypeOptions |
MiterOptions.ClosedCornerTypeOptions.CLOSED
corner is closed completely
|
static MiterOptions.ClosedCornerTypeOptions |
MiterOptions.ClosedCornerTypeOptions.NONE
Corner is not closed
|
static MiterOptions.ClosedCornerTypeOptions |
MiterOptions.ClosedCornerTypeOptions.OPEN
corner is open
|
static MiterOptions.ClosedCornerTypeOptions |
MiterOptions.ClosedCornerTypeOptions.UCUTOUT
corner has a U shaped cutout in it
|
static MiterOptions.ClosedCornerTypeOptions |
MiterOptions.ClosedCornerTypeOptions.VCUTOUT
corner has a V shaped cutout in it
|
Modifier and Type | Method and Description |
---|---|
MiterOptions.ClosedCornerTypeOptions |
MiterOptions.closedCornerType()
Returns the closed corner option type.
|
static MiterOptions.ClosedCornerTypeOptions |
MiterOptions.ClosedCornerTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MiterOptions.ClosedCornerTypeOptions |
MiterOptions.ClosedCornerTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MiterOptions.ClosedCornerTypeOptions[] |
MiterOptions.ClosedCornerTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MiterOptions.setClosedCornerType(MiterOptions.ClosedCornerTypeOptions cutType)
Sets the closed corner option type.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.