Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static MiterOptions.PositionOptions |
MiterOptions.PositionOptions.BOTH
miter is done both at beginning and ending
|
static MiterOptions.PositionOptions |
MiterOptions.PositionOptions.END
miter is done at the ending
|
static MiterOptions.PositionOptions |
MiterOptions.PositionOptions.NONE
no miter
|
static MiterOptions.PositionOptions |
MiterOptions.PositionOptions.START
miter is done at the beginning
|
Modifier and Type | Method and Description |
---|---|
MiterOptions.PositionOptions |
MiterOptions.position()
Returns the position of miter.
|
static MiterOptions.PositionOptions |
MiterOptions.PositionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MiterOptions.PositionOptions |
MiterOptions.PositionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MiterOptions.PositionOptions[] |
MiterOptions.PositionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MiterOptions.setPosition(MiterOptions.PositionOptions miterPosition)
Sets the position of miter.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.