Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static ThreeBendCornerBuilder.OriginTypes |
ThreeBendCornerBuilder.OriginTypes.BEND_CENTER
The relief origin will be at the intersection of first bend's centerline and bisector of corner angle.
|
static ThreeBendCornerBuilder.OriginTypes |
ThreeBendCornerBuilder.OriginTypes.CORNER_POINT
The relief origin will be at the corner point.
|
Modifier and Type | Method and Description |
---|---|
ThreeBendCornerBuilder.OriginTypes |
ThreeBendCornerBuilder.originType()
Returns the relief origin used for circular, u and v cutout corner treatments.
|
static ThreeBendCornerBuilder.OriginTypes |
ThreeBendCornerBuilder.OriginTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThreeBendCornerBuilder.OriginTypes |
ThreeBendCornerBuilder.OriginTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThreeBendCornerBuilder.OriginTypes[] |
ThreeBendCornerBuilder.OriginTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThreeBendCornerBuilder.setOriginType(ThreeBendCornerBuilder.OriginTypes originType)
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.