Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static AeroLighteningCutoutBuilder.Types |
AeroLighteningCutoutBuilder.Types.HOLE |
static AeroLighteningCutoutBuilder.Types |
AeroLighteningCutoutBuilder.Types.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
AeroLighteningCutoutBuilder.Types |
AeroLighteningCutoutBuilder.type()
Returns the feature type
License requirements: None. |
static AeroLighteningCutoutBuilder.Types |
AeroLighteningCutoutBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AeroLighteningCutoutBuilder.Types |
AeroLighteningCutoutBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AeroLighteningCutoutBuilder.Types[] |
AeroLighteningCutoutBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AeroLighteningCutoutBuilder.setType(AeroLighteningCutoutBuilder.Types type)
License requirements: aero_sheet_metal ("Aerospace Sheet Metal") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.