public static class AeroLighteningCutoutBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HOLE |
static int |
_USER_DEFINED |
static AeroLighteningCutoutBuilder.Types |
HOLE |
static AeroLighteningCutoutBuilder.Types |
USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
static AeroLighteningCutoutBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AeroLighteningCutoutBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AeroLighteningCutoutBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final AeroLighteningCutoutBuilder.Types HOLE
public static final AeroLighteningCutoutBuilder.Types USER_DEFINED
public static final int _HOLE
public static final int _USER_DEFINED
public static AeroLighteningCutoutBuilder.Types valueOf(int value)
public static AeroLighteningCutoutBuilder.Types valueOf(String name)
public static AeroLighteningCutoutBuilder.Types[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.