Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BendBuilder.BendLocationOptions |
BendBuilder.BendLocationOptions.CENTER_LINE |
static BendBuilder.BendLocationOptions |
BendBuilder.BendLocationOptions.INNER_MOLD_LINE |
static BendBuilder.BendLocationOptions |
BendBuilder.BendLocationOptions.MATERIAL_INSIDE |
static BendBuilder.BendLocationOptions |
BendBuilder.BendLocationOptions.MATERIAL_OUTSIDE |
static BendBuilder.BendLocationOptions |
BendBuilder.BendLocationOptions.OUTER_MOLD_LINE |
Modifier and Type | Method and Description |
---|---|
BendBuilder.BendLocationOptions |
BendBuilder.bendLocation()
Returns the Bend Location (Material Side)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static BendBuilder.BendLocationOptions |
BendBuilder.BendLocationOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendBuilder.BendLocationOptions |
BendBuilder.BendLocationOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendBuilder.BendLocationOptions[] |
BendBuilder.BendLocationOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BendBuilder.setBendLocation(BendBuilder.BendLocationOptions bendLocation)
Sets the Bend Location (Material Side)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.