Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static DrawnCutoutBuilder.DepthTypeOptions |
DrawnCutoutBuilder.DepthTypeOptions.SECTION_NORMAL_SIDE
Drawn Cutout punched on the side of the section normal.
|
static DrawnCutoutBuilder.DepthTypeOptions |
DrawnCutoutBuilder.DepthTypeOptions.SECTION_REVERSE_NORMAL_SIDE
Drawn Cutout punched on the side opposite to that of the section normal
|
Modifier and Type | Method and Description |
---|---|
DrawnCutoutBuilder.DepthTypeOptions |
DrawnCutoutBuilder.depthType()
Returns the Direction in which the Drawn Cutout is punched.
|
static DrawnCutoutBuilder.DepthTypeOptions |
DrawnCutoutBuilder.DepthTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawnCutoutBuilder.DepthTypeOptions |
DrawnCutoutBuilder.DepthTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawnCutoutBuilder.DepthTypeOptions[] |
DrawnCutoutBuilder.DepthTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawnCutoutBuilder.setDepthType(DrawnCutoutBuilder.DepthTypeOptions depthType)
Sets the Direction in which the Drawn Cutout is punched.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.