Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static FlangeBendPropertiesBuilder.WidthOptions |
FlangeBendPropertiesBuilder.WidthOptions.AT_CENTER |
static FlangeBendPropertiesBuilder.WidthOptions |
FlangeBendPropertiesBuilder.WidthOptions.AT_END |
static FlangeBendPropertiesBuilder.WidthOptions |
FlangeBendPropertiesBuilder.WidthOptions.FROM_BOTH_ENDS |
static FlangeBendPropertiesBuilder.WidthOptions |
FlangeBendPropertiesBuilder.WidthOptions.FROM_END |
static FlangeBendPropertiesBuilder.WidthOptions |
FlangeBendPropertiesBuilder.WidthOptions.FULL |
Modifier and Type | Method and Description |
---|---|
static FlangeBendPropertiesBuilder.WidthOptions |
FlangeBendPropertiesBuilder.WidthOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBendPropertiesBuilder.WidthOptions |
FlangeBendPropertiesBuilder.WidthOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBendPropertiesBuilder.WidthOptions[] |
FlangeBendPropertiesBuilder.WidthOptions.values()
Returns an array that contains the values for this enum.
|
FlangeBendPropertiesBuilder.WidthOptions |
FlangeBendPropertiesBuilder.widthOption()
Returns the width option
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
FlangeBendPropertiesBuilder.setWidthOption(FlangeBendPropertiesBuilder.WidthOptions widthOption)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.