Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static FlatSolidBuilder.OrientationType |
FlatSolidBuilder.OrientationType.CSYS
transform flat solid body as per orientation defined by CSYS
|
static FlatSolidBuilder.OrientationType |
FlatSolidBuilder.OrientationType.DEFAULT
do not orient flat solid body
|
static FlatSolidBuilder.OrientationType |
FlatSolidBuilder.OrientationType.EDGE
transform flat solid body as per orientation defined by edge
|
Modifier and Type | Method and Description |
---|---|
FlatSolidBuilder.OrientationType |
FlatSolidBuilder.orientation()
Returns the option which decides if the flattened solid will be transformed to Absolute CSYS.
|
FlatSolidBuilder.OrientationType |
FlatPatternBuilder.orientation()
Returns the option which decides if the flattened solid will be transformed to Absolute CSYS.
|
static FlatSolidBuilder.OrientationType |
FlatSolidBuilder.OrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlatSolidBuilder.OrientationType |
FlatSolidBuilder.OrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlatSolidBuilder.OrientationType[] |
FlatSolidBuilder.OrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlatSolidBuilder.setOrientation(FlatSolidBuilder.OrientationType orientation)
Sets the option which decides if the flattened solid will be transformed to Absolute CSYS.
|
void |
FlatPatternBuilder.setOrientation(FlatSolidBuilder.OrientationType orientation)
Sets the option which decides if the flattened solid will be transformed to Absolute CSYS.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.