public static class FlatSolidBuilder.OrientationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CSYS
transform flat solid body as per orientation defined by CSYS
|
static int |
_DEFAULT
do not orient flat solid body
|
static int |
_EDGE
transform flat solid body as per orientation defined by edge
|
static FlatSolidBuilder.OrientationType |
CSYS
transform flat solid body as per orientation defined by CSYS
|
static FlatSolidBuilder.OrientationType |
DEFAULT
do not orient flat solid body
|
static FlatSolidBuilder.OrientationType |
EDGE
transform flat solid body as per orientation defined by edge
|
Modifier and Type | Method and Description |
---|---|
static FlatSolidBuilder.OrientationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlatSolidBuilder.OrientationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlatSolidBuilder.OrientationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final FlatSolidBuilder.OrientationType DEFAULT
public static final FlatSolidBuilder.OrientationType EDGE
public static final FlatSolidBuilder.OrientationType CSYS
public static final int _DEFAULT
public static final int _EDGE
public static final int _CSYS
public static FlatSolidBuilder.OrientationType valueOf(int value)
public static FlatSolidBuilder.OrientationType valueOf(String name)
public static FlatSolidBuilder.OrientationType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.