Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static TabBuilder.SectionSideOptions |
TabBuilder.SectionSideOptions.LEFT
Side pointed to by the inverse of the tangent cross normal vector
|
static TabBuilder.SectionSideOptions |
TabBuilder.SectionSideOptions.RIGHT
Side pointed to by the tangent cross normal vector
|
Modifier and Type | Method and Description |
---|---|
TabBuilder.SectionSideOptions |
TabBuilder.materialSide()
Returns the material side value of secondary tab
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static TabBuilder.SectionSideOptions |
TabBuilder.SectionSideOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TabBuilder.SectionSideOptions |
TabBuilder.SectionSideOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TabBuilder.SectionSideOptions[] |
TabBuilder.SectionSideOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TabBuilder.setMaterialSide(TabBuilder.SectionSideOptions sectionSide)
Sets the material side value of secondary tab
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.