Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static DrawnCutoutBuilder.SidewallTypeOptions |
DrawnCutoutBuilder.SidewallTypeOptions.INSIDE
the outerface of the drawn cutout side walls coincides with the section outline.
|
static DrawnCutoutBuilder.SidewallTypeOptions |
DrawnCutoutBuilder.SidewallTypeOptions.OUTSIDE
the innerface of the drawn cutout side walls coincides with the section outline.
|
Modifier and Type | Method and Description |
---|---|
DrawnCutoutBuilder.SidewallTypeOptions |
DrawnCutoutBuilder.sidewallType()
Returns the side where the material must be added to the Drawn Cutout.
|
static DrawnCutoutBuilder.SidewallTypeOptions |
DrawnCutoutBuilder.SidewallTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawnCutoutBuilder.SidewallTypeOptions |
DrawnCutoutBuilder.SidewallTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawnCutoutBuilder.SidewallTypeOptions[] |
DrawnCutoutBuilder.SidewallTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawnCutoutBuilder.setSidewallType(DrawnCutoutBuilder.SidewallTypeOptions sidewallType)
Sets the side where the material must be added to the Drawn Cutout.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.