Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static AdvancedFlangeBuilder.LengthReferences |
AdvancedFlangeBuilder.LengthReferences.DIN6935 |
static AdvancedFlangeBuilder.LengthReferences |
AdvancedFlangeBuilder.LengthReferences.INSIDE |
static AdvancedFlangeBuilder.LengthReferences |
AdvancedFlangeBuilder.LengthReferences.OUTSIDE |
static AdvancedFlangeBuilder.LengthReferences |
AdvancedFlangeBuilder.LengthReferences.WEB |
Modifier and Type | Method and Description |
---|---|
AdvancedFlangeBuilder.LengthReferences |
AdvancedFlangeBuilder.lengthReference()
Returns the length reference
License requirements: None. |
static AdvancedFlangeBuilder.LengthReferences |
AdvancedFlangeBuilder.LengthReferences.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AdvancedFlangeBuilder.LengthReferences |
AdvancedFlangeBuilder.LengthReferences.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AdvancedFlangeBuilder.LengthReferences[] |
AdvancedFlangeBuilder.LengthReferences.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AdvancedFlangeBuilder.setLengthReference(AdvancedFlangeBuilder.LengthReferences lengthReference)
License requirements: adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.